2012-03-13 3:43 AM
ADC DMA problem
2012-03-13 10:04 AM
At the moment, I am assuming that clocks and GPIOs are correctly initialized.
I need a better description of the relationship between sampling trigger and square wave frequency. Is the sampling trigger frequency 1 MHz ? What is the square wave frequency ? How are you sorting out the triple conversion results to reconstruct the square wave at the trigger frequency ? A signal 1 V pp suggests the signal is sometimes negative. Do you really mean that the signal goes from 0.5 mV to 1 V ? Cheers, Hal2012-03-19 5:36 AM
Hello,
Excuse me for the late reply I managed to fix the problem which is due to a little error on the clock configuration. Thanks for your reply.