STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wakeup from timer interrupt

Posted on January 24, 2013 at 17:54Hi allI  am using STM32  and trying to make the  periodic  wake up  of the CPU from low power sleep mode , by interrupt from TIMER 9 , and I see the following strange behavior: I    succeeded to wake up the CPU fro...

genadyk by Associate II
  • 2914 Views
  • 5 replies
  • 0 kudos

STM32_USBD_OTG VCP example explanation

Posted on March 17, 2013 at 12:51Hi all, I am a beginner to USB and after some days of reading USB OTG library and RM0033 in the scope of getting started with USB. I'll to try to explain the virual com port example in my own words and fore w/o garan...

STM32F103RB I2C problem

Posted on March 19, 2013 at 13:12 Hi, I am trying to comunicate with MCP23016 by i2c and i am using STM32F103RB with uVision 4. The problem is that if I send 0x40 is the same if I send 0x41. Its the red mark on the code. My code is: ...

0690X0000060542QAA.png 0690X000006054MQAQ.png 0690X0000060543QAA.png
felipe by Associate II
  • 2174 Views
  • 5 replies
  • 0 kudos

Flash loader demonstrator V2.6.0 version error

Posted on March 18, 2013 at 11:09I have a project with STM32F1, which is well programmed with the 2.2.0 version of STMFlashLoader.exe, but with the versions 2.5.0 and 2.6.0 the system gives message: bad parameter [files\STMicroelectronics\Software''...

var2 by Associate III
  • 2706 Views
  • 5 replies
  • 0 kudos

STM32F0 IDE Setup & Blinking LED Video Tutorial

Posted on March 18, 2013 at 18:41Hey all, I made a video tutorial of how to blink an LED using the CooCox IDE with the STM32F0 Discovery board. I'm using the CooCox free open source IDE in order to avoid any type of code size limitations. Youtube li...

Flash Read and Write Problem

Posted on March 19, 2013 at 10:40Hi,      I want to display 2 parameters(ID and BD) value on seven segment display. The values will be dynamically changed, so every time I want to write these 2 byte of values on FLASH memory and every power ON or Sy...

ss2 by Associate II
  • 6453 Views
  • 11 replies
  • 0 kudos

STM32F3Discovery, replaced MCU with STM32F407VGT6

Posted on March 21, 2013 at 00:23Hi,I have a STM32F3Discovery eval. board which I used to build an IMU controlled by a computer through Graphical User Interface. This is an excellent board (9 Degrees of Freedom) and it is a good way to start.I have ...

ebader18 by Associate
  • 1503 Views
  • 2 replies
  • 0 kudos

problem on 3V3 IO to drive 5V chipset with SPI

Posted on March 19, 2013 at 16:07Dear everyone,     I met a problem when I try to use the SPI (3.3V) to drive the meganetic isolation ADum2400 which is powered by 5V.The SPI pin are remapped to SPI3 (PC10, PC11, PC12) and the CS pin are remapped to ...

xinjin by Associate II
  • 3631 Views
  • 5 replies
  • 0 kudos