STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC conversion question

Posted on April 13, 2013 at 17:39I have a potential divider circuit set up using the 3V and GND pins on the discovery board and two 100ohm pots, I measure a constant divided voltage of 1.25 (from ground to the ADC input) but when I debug in Uvision ...

bee2 by Associate II
  • 3520 Views
  • 10 replies
  • 0 kudos

NEW Operator under µVision 4

Posted on April 15, 2013 at 19:55Hello Community, i´m having a stm32f3Discovery under the Keil´s µVision4 Compiler programming in c++. I got to the point, where i could use the ''NEW''  operator. To be honest, i have no idea, what is really goin...

Detecting Rising and Falling edges

Posted on April 18, 2013 at 09:21Hi, I am using an STM32L151VB part in a custom board. Is there any way to detect if an interrupt has been caused by a rising or a falling edge. I looked around in the reference manual and didnt find anything. I need ...

adithya2 by Associate II
  • 2931 Views
  • 2 replies
  • 0 kudos

eeprom 24c02 on stm32f0

Posted on April 17, 2013 at 11:58The original post was too long to process during our migration. Please click on the attachment to read the original post.

pietro2 by Associate II
  • 1553 Views
  • 1 replies
  • 0 kudos

FreeRtos ARM

Posted on April 16, 2013 at 15:15Does someone know where can i find a tutorial about configuring a FreeRTOS ARM Cortex-M4F demo application that targets an STMicroelectronics STM32F40XX microcontroller using eclipse please ? http://www.st.com/intern...

ST LINK error

Posted on April 17, 2013 at 08:53Since yesterday, i can't establish a ST LINK connection with my STM32L1-Discovery board. I've tried it in CrossWorks on my MacBook, the error was 'ST-LINK LOG'. After that, I've tried it on my windows 7 pc with ST LI...

USART ore after 8 bytes always

Posted on December 28, 2012 at 01:21 Hello All, I'm sending data over a bluetooth device to the stm32 discovery board on usart 2. Everything is great unless I send a large amount of data (80 bytes). If I send this large amount I only end up ...

STANDBY and RTC

Posted on April 15, 2013 at 15:14Hi Again ; In my application stm32f407 will enter stanfby mode then should wake up by 2 methods ; a rising edge on the PA0( wakeup _pin) and an alarm occurs everyday one time .. the first one I thing I will not get...

sami by Associate II
  • 3593 Views
  • 9 replies
  • 0 kudos