Question
Best bluetooth module to use
Posted on April 29, 2012 at 22:17
Hi all,
I am currently using the STM3210C evaluation board to implement a prototype for a project I am currently busy with, and I am at the point where I need to add Bluetooth capability to my board. In essence what I am trying to achieve is to stream the data from the STM3210C to another computer which is situated away from the STM3210C. I was thinking of using a Bluetooth module as from what I can see on the net, there are Bluetooth modules which can be used to make ''wireless serial cables''. So the idea is to use my eval board to interface to a Bluetooth module using the USART (RS232); and then pair the Bluetooth module to my laptop to get the information off the eval board. I was hoping that this forum could point me towards an appropriate module which someone has possibly used in a project before, and that is easy to interface with the STM32 range. Thanks in advance for any help which you guys can offer. Regards, Tony #rs232 #stm3210c #stm3 #bluetooth