STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usart hangs when nothing connected

Posted on April 14, 2013 at 00:00If I dont have anything on the usart port then it hangs when sending data. I have a ''debug'' usart output that I only want to use sometimes. But if I dont have anything connected then it will sit and hang here PUTCH...

Hard fault at misaligned memcpy memset

Posted on April 15, 2013 at 16:11Already posted this on Keil Website, it was tested with STM32F100, therefore:we made some simple tests with STM32F100 Value Line Eval Board://--------------------------------------------------------------------------...

STM32F4Discovery VCP Problem

Posted on April 18, 2013 at 18:44Hello,I want to test http://www.mediafire.com/?0ghzhc6jgn90u4k of VCP on STM32F4 Discovery board.But in building the project the following error occurs.warning: implicit declaration of function 'VCP_dataTx' is invali...

STM32F1x SPI can't reset/re-sync after a data error

Posted on April 19, 2013 at 16:34I have been looking at using the SPI peripheral on an STM32F103VET6 MCU. I am intending to use SPI to network 3 MCU's on a single PCB as I need to support 12 duplex high speed USARTS for a large RS485 project. I ran...

DMA STM32F4 with external SRAM and SSD1963 on FSMC

Posted on April 15, 2013 at 15:04Hello, I'm trying to configure DMA2 stream 0 to do a transfer from external SRAM on the FSMC to a SSD1963 Display controller also on the FSMC. This is my code can't seem to get it working, I assume this is possible? ...

keil problem Error #136

Posted on April 18, 2013 at 18:41Hello I have a struct in my code ;typedef struct { unsigned char  volume; unsigned char  l_bat; unsigned char  h_bat; unsigned char  rtc; unsigned char  pace; unsigned char  child;  unsigned char date; unsigned cha...

sami by Associate II
  • 2029 Views
  • 6 replies
  • 0 kudos

gnu math library about stm32f4

Posted on April 19, 2013 at 05:54I want to use stm32f4 to control my accelerometer. And I need to use the acceleration value to calculate the rotation degree. So I need sqrt() and acos() function from math.h . I used gnu tool with st-link to finish ...

ctc.ctc by Associate II
  • 1256 Views
  • 1 replies
  • 0 kudos

STM32F4 Serial Interrupts Crash

Posted on April 09, 2013 at 19:01The original post was too long to process during our migration. Please click on the attachment to read the original post.

jdp6q5 by Associate II
  • 3394 Views
  • 5 replies
  • 0 kudos

STM32F4 DISCOVERY with linux

Posted on April 05, 2013 at 17:26Hello, Am trying tocompile STM32 examples in linux but i want to know if i have to install some drivers so that the linux can recognize it. Best Regards, Dorra