cancel
Showing results for 
Search instead for 
Did you mean: 

5.7'' TFT display 640X480 16bit FSMC part number

sri1904
Associate
Posted on May 08, 2012 at 12:08

For my current project we are using a development board of powerAVR. It has a 3.5� TFT touchpanel with resolution 320x240, using 16bit FSMC bus for communication. But I need to have implement it on a 5.7� TFT with resolution 640x480.

We have been searching to find  a suitable part which is FSMC compatible, but with no success till now. can anyone provide the details regarding the part number of the same.

The controller on the development board is STM32F103ZE and the display controller is SSD1963. It will be very appreciated if the display controller is the same.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
balmukund66
Associate II
Posted on May 09, 2012 at 07:50

For your Requirment IS64WV102416BLL will be sufficient.

balmukund66
Associate II
Posted on May 10, 2012 at 06:18

TFT Part no is 

AM-640480GTMQW-00H

sri1904
Associate
Posted on May 10, 2012 at 10:57

Thanks for reply:-)

but i actually need a Touchpanel integrated TFT. LCD

it should be 640x480, 5.7'' and 16bit FSMC compatible.

if it is controlled by SSD1963 display controller it will be more helpful to me.