Skip to main content
kb_it
Associate
July 31, 2012
Question

Placing Stack and Heap at specific location

  • July 31, 2012
  • 0 replies
  • 1055 views
Posted on July 31, 2012 at 20:39

I have the following scatter file,

LR_IROM1 0x08000000 0x00100000
{ ; load region size_region
;ARM_LIB_HEAP 0x20000000 EMPTY 0x200{} ; Heap starts at 1MB
; and grows upwards
;ARM_LIB_STACK 0x20020000 EMPTY -0x400{} ; Stack space starts at the end
; of the 2MB of RAM
; And grows downwards for 32KB
ER_IROM1 0x08000000 0x00100000
{ ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x20000000 0x00020000
{
.ANY3 (+RW +ZI)
}
RW_IRAM2 0x10000000 0x00010000
{
.ANY2 (+RW +ZI)
}
RW_RAM1 0x68000000 0x00080000
{ ; RW data
.ANY1 (+RW +ZI)
}
}

If I uncomment the two Stack and Heap directives and remove the priorities of the .ANY, the linker puts the Stack in RAM1 which is external RAM. What is the correct syntax to specify the location of the Stack.

I am using the ''startup_stm32f4xx.s'' which contains Stack initialisation,

;*******************************************************************************
; User Stack and Heap initialization
;*******************************************************************************
IF :DEF:__MICROLIB
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
ELSE
IMPORT __use_two_region_memory
EXPORT __user_setup_stackheap
__user_setup_stackheap
LDR R0, = Heap_Mem
LDR R1, =(Stack_Mem + Stack_Size)
LDR R2, = (Heap_Mem + Heap_Size)
LDR R3, = Stack_Mem
BX LR
ALIGN
ENDIF

END

The ARM_LIB_STACK directive is taken straight from the Keil help.

regards

Konrad #stack-scatter-stm32f4
This topic has been closed for replies.