STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 stuck on read protect

Hi, I am using STMH755ZI chip and i have a custom board created using this. I have code which receives a character through UART and jumps to DFU mode for flashing. I am not using ST LINK and in case of emergency, i kept BOOT0 pin open so that i can g...

kps98_0-1729412353225.png kps98_1-1729412376730.png
kps98 by Associate III
  • 3235 Views
  • 5 replies
  • 0 kudos

SPL support for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1?

Hello.Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible?I need to continue to use the Standard Peripheral Library (SPL) to utilize the existing code.If there is a way to create or convert the project by X-CUBE-MCS...

Writing Option Bytes on STM32F1

Hello,Im developing an program that controls an ST-Link to flash an STM32F1. The program needs to be able to remove RDP on the MCU its trying to flash.Im doing the following steps:1) Unlocking Flash - confirmed working (registers confirm)2) Unlocking...

guandast_2-1729788721514.png guandast_1-1729788647355.png
guandast by Associate II
  • 2336 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G474 Unable to initialize more than one ADC

Hi All,I'm trying to setup 2 ADCs in continous mode but I'm failing miserably. In CubeMX I set the first ADC in continuous mode, triggered by software, then HAL_ADC_Start_IT(&hadc1); and it works as expected (I have a callback to read the value).Then...

aldoir by Associate
  • 1755 Views
  • 2 replies
  • 0 kudos

STM32 I2C wont work without debugger

Posted on August 28, 2013 at 12:45Hi all!Im currently working with a project that should read data from sensors using the I2C bus.When i am using a debugger to start the program it runs at it should. Reading sensor values and putting out the data on...

ojoel by Associate
  • 7180 Views
  • 11 replies
  • 2 kudos

Resolved! UART HMI Display Receive-Transmit Issue

Hi,I am Faruk.What i am trying to do is, sending data that i collacted from ADC Ports to Nextion HMI Display. Also at the same time i am getting signals from buttons on the Nextion HMI Display. I use UART pins of Nextion HMI Display. 5V RX TX GND.If ...

frkdkk by Associate II
  • 4223 Views
  • 4 replies
  • 0 kudos

Nextion HMI UART Issue

Hi,I am using an STM32F407 Evaluation Board in my project, along with a Nextion HMI Display that communicates with the MCU over UART.In this project, I send data every 1 second using a TIM interrupt with UART Polling Mode, and I receive data from the...

frkdkk1 by Associate
  • 5768 Views
  • 3 replies
  • 1 kudos

STM32U535CB for Bicycle Computer Application

Dear STM CommunityI am reaching out on behalf of our development team, as we are in the process of selecting an appropriate microcontroller for a bicycle computer application. We are considering the STM32U535CB for its ultra-low power consumption, ro...