STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405RG USB FS unexpected Interrupt

Posted on June 17, 2013 at 18:30I build my own STM32F405RG Stamp and try now to get the USB FS running. For to make good progress I use the libraries, which are available for the stm32F407 Discovery. I use Atollic True Studio Lite and ST-Link/V2 SWD...

mgmv05 by Associate II
  • 1093 Views
  • 1 replies
  • 0 kudos

STM32 Accelometer

Posted on June 17, 2013 at 17:07hello people i'm using IAR  IDE and i'm trying to make a program which get accelo values (x and y) and put them on lcd  this is my code and it didnt work i dont know why: ****************************** #include ''stm...

On board ST-LINK and Windows 8

Posted on November 29, 2012 at 13:34Hello,I have same problem with my ST Discovery board on Windows 8. After I connect board to PC, windows was trying to install driver - but unsuccessful because driver files does´t contain a digital signature. In ...

hospodar by Associate III
  • 1444 Views
  • 3 replies
  • 0 kudos

systick always 3 times what it should be

Posted on June 18, 2013 at 05:03I've tested the example systick app and it worked, but my (keil) app will not work. I'm just trying to blink a light on a 2 sec interval, super frustrating.the project settings have the system clock at 25mhz. I'm usin...

STM32F3 Discovery File Compatibility

Posted on June 17, 2013 at 17:43I'm currently working with a STM32F3-Discovery board which has the STM32F303VC microcontroller on it.  I'm planning on eventually using the STM32F373C8 on my board, but I want to test out some code and get comfortable...

mattfox by Associate II
  • 978 Views
  • 2 replies
  • 0 kudos

Setting SPI1 freq for SD card = 24Mhz

Posted on June 17, 2013 at 12:32I am using STM32F205 with 120Mhz interanl PLL(HSI).I have to interface SD Card on SPI with <= 24Mhz. Problem is with 120Mhz sysclk I can only obtain SPI-30Mhz(can't use of SD), 15Mhz(too slow)and other lower freq.Now ...

Blinking LED based on IWDG counter

Posted on June 15, 2013 at 13:38Hi, In our system, our main code loop repeats every 12 seconds and refreshs the watchdog counter. When refreshing the counter, I toggle an LED. The only problem is the blink period. I would lke the watchdog running LE...

stenasc by Senior
  • 2832 Views
  • 9 replies
  • 0 kudos

Datasheet correct for LQFP64 F37x or not?

Posted on June 15, 2013 at 03:44I'm looking for confirmation (first hand knowledge, please -- speculation is usless) that PA3 on the F37x and F38x are in fact at pin 18 and not on pin 17 as it is for all the other LQDP64-packaged F1xx, F2xx, F3xx, a...

gfuehrer by Associate II
  • 1332 Views
  • 2 replies
  • 0 kudos

Self-test library for STM32F2xx?

Posted on October 05, 2012 at 09:45Hello, for STM32F1xx a self-test library is available as described in AN3307. Is a similar library available for STM32F2xx? Or can the same library be adapted for STM32F2xx? Bodo

extern by Associate
  • 1524 Views
  • 2 replies
  • 0 kudos