STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with connection

Posted on August 12, 2013 at 15:31Hello everyone! I have annoying trouble with my STM32F0 Discovery. After using GPIO->MODER command is displayed Connect failed, check config and cable connection . What is the reason of that issue and how can I fix ...

michal by Associate
  • 930 Views
  • 1 replies
  • 0 kudos

Store user data in STM32 Flash or Rom

Posted on August 12, 2013 at 08:10Hello everyone, I am newbie in this forum so please forgive me for any noob questions. My application requires to save 4 double variables offline for next time usage, I think my data is too small to make us use a SD...

cenakhoa by Associate
  • 1274 Views
  • 1 replies
  • 0 kudos

stm32f4discovery, continues adc, noise

Posted on August 08, 2013 at 05:14 I'm sorry, that's probably quite a beaten topic :( I have continues mode ADC running on stm32f4discovery board. static void ADC_Config(void) { ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef...

arro239 by Senior
  • 2317 Views
  • 6 replies
  • 0 kudos

FFT function oddities

Posted on August 09, 2013 at 10:42I'm using the ''arm_cfft_radix4_f32(&S, FFTData); '' function to obtain the FFT of an array and then inverse it back after some processing. I have things working, to a point, but with some odd restrictions. Firstl...

STM32F4 USART PROBLEM

Posted on August 09, 2013 at 20:18Hello, everyone.  I am currently playing around with the USART without standard peripheral lib provided by ST (using CMSIS only) and my code strangely works in one MDK project and does not work in another MDK projec...

ran2 by Associate III
  • 2108 Views
  • 4 replies
  • 0 kudos

AT commands for HTTP

Posted on August 12, 2013 at 09:10Hi all,I am using HILO GSM modem of Sagem. It supports HTTP feature. I am implenting that feature in my device but i am facing problem while using POST and GET commands related to HTTP. I am using AT commands to imp...

manoj23 by Associate II
  • 883 Views
  • 0 replies
  • 0 kudos

Quadrature Encoder Channels

Posted on August 09, 2013 at 20:11I'm working with the STM32F3 Discovery board.  I'm wondering if it is possible to use a timer in encoder interface mode with the signals coming in on Channels 1 and 4.  Do you have to use channels 1 and 2?  Does the...

mattfox by Associate II
  • 1435 Views
  • 2 replies
  • 0 kudos

Current Consumption of STM32L-DISCOVERY in low Power Modes

Posted on August 11, 2013 at 19:23Hi, I am using the STM32L-DISCOVERY evaluation board, and I made JP1 off as per the below instructions from the evaluation board user manual:  JP1 OFF: the STM32L152 is directly powered, IDD measurement circuit is b...

aa_talaat by Associate II
  • 1044 Views
  • 1 replies
  • 0 kudos

HSI vs. HSE crystals

Posted on August 11, 2013 at 19:01I've been looking at some board designs that I've found online, and it looks like some people include an external 8 MHz crystal in a resonator to run their clock.  I'm wondering what the benefit of using this extern...

mattfox by Associate II
  • 1950 Views
  • 3 replies
  • 0 kudos

GNU gcc toolchain on linux

Posted on August 10, 2013 at 00:33Hi all,I've been playing with different peripheral examples of STM32L-Discovery on MDK-ARM (Keil) environment.  Recently I'd like to move to linux with GNU gcc tool chain.  I had a hard time learning to write a Make...