STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Coocox and the stm32f427vit6

Posted on September 12, 2013 at 11:33Hello,I was using Coocox and the STM32F407VGT6 and now I move to the new STM32F427VIT6. This microcontroller is not supported by Coocox, I have to select I'm using a STM32F407 but it works with that config (I can...

When I touch the SCL pin with my finger the SPI works

Posted on September 11, 2013 at 17:32Hello,I programmed a LCD screen with SPI on a prototype and everything was working fine. But I mounted the screen on the final PCB and now I have a problem: the screen didn't understand the datas I send to it. Th...

J-Link and STM32F103VET6 issue

Posted on September 15, 2013 at 01:18Guys I got : Guys, I got error on reading STM32 : What should I fix ? thanks **JLink Warning: Identified core does not match configuration. (Found: None, Configured: Cortex-M3) * JLink Info: TotalIRLen = 9, IRPri...

Startup file and interrupts

Posted on September 14, 2013 at 21:34  The original post was too long to process during our migration. Please click on the attachment to read the original post.

eltar by Associate III
  • 2049 Views
  • 2 replies
  • 0 kudos

Help with SDIO

Posted on March 04, 2013 at 18:09Hi guys. First of all, sorry if my english is bad. I have a problem configuring a uSD and SDIO port. I'm using the ST SDIO example for STM32f4 discovery board and I cant comunicate with de micro SD. I checked the pin...

STM3240G-EVAL Help me please!

Posted on October 06, 2012 at 11:50Hi, I just bought an evaluation board STM3240G-EVALI tried to modify the example provided by ST called ''ADC3_DMA'' but I could not change the pin from what I acquire the signal For example I wanted to go from pin ...

fullcaos by Associate II
  • 6486 Views
  • 13 replies
  • 0 kudos

DCMI interface + camera module

Posted on September 12, 2013 at 20:27Hi,I am trying to interface the OV5642 camera module with the STM32F4 microcontroller. So I wanted to ask about the XCLK signal in the camera, should it stay NC, or should I connect it to a clock (10Mhz to 24Mhz ...

STM32F100 ADC - read channels in scan mode

Posted on September 13, 2013 at 21:03 I can get the value from one channel of ADC but now if I use the scan mode how can I get each value? thanks :) #include <stm32f10x.h> #include <stm32f10x_gpio.h> #include <stm32f10x_rcc.h> #inc...

ee06091 by Associate III
  • 936 Views
  • 1 replies
  • 0 kudos

STM32F1 ADC - Only works the first 2/3 times

Posted on September 12, 2013 at 19:27 Hi, I'm trying the ADC on STM32VLDiscovery. #include <stm32f10x.h> #include <stm32f10x_gpio.h> #include <stm32f10x_rcc.h> #include <stm32f10x_tim.h> #include <stm32f10x_adc.h> #include <misc.h...

ee06091 by Associate III
  • 1551 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.