HiI wanted to test ST MotorControl Workbench for experimenting with brushless motors, I have installed and tested the MotorControl Workbench 6.2.1 and MotorControl Workbench 5.4.8 on win 11 and both of them would fail to generate the projects out of ...
Hi,I have an external SPI 8 channel ADC which is connected to the STM32,one of timers would generate a 32KHz 50% pwm signal which is connected to the ADC convert pin, the ADC has a busy pin which is connected to the EXTI0 of the MCU.The plan is to us...
Hi,I want to use STM32H750XBH6 part with a LCD of 24bit @1024x600 resolution, Do you have any Idea about the performance? is it slow or can it do the job?
Hi,I have a screen that no other screen would transition to it with the help of interactions in the designer,I know I can transition to other screens with the help of this functionstatic_cast<FrontendApplication*>(Application::getInstance())->goto...
Hi,I have a new project based on STM32H750VB, everything works, But when I make some transition between screens, it would just swap screens almost instantly! but the same code works nicely in simulation, what's wrong with the transitions?
Also why It does not allow to use FOC algorithm! it says it has no current sense option, But clearly there is "features": [{"name": "CurrentSensing","type": "CurrentSensing","tRise": 1000,"hwVariants": [{"type": "SingleShunt_AmplifiedCurrents_noOffs...
Hi cerdic HI have installed a fresh MotorControl Workbench_6.3.0 and used my mySTM32G030KT6.json file to generate a simple 6 step design, Now when I hit generate design it would make the design and it says the design has some errors when I hit Genera...
Maybe it's time to search or investigate for other manufacturers like NXP to see what they had to offer, since I can not get even a normal response from ST or other users, does any one here even done a custom board design using the ST MotorControl ...