cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 adc problem

ctc.ctc
Associate II
Posted on April 21, 2013 at 14:58

I would like to use stm32f4 to measure a battery voltage, like AA1.5v 

I connect the postive line to PC5 and gnd line to GND.

I reference the example code on the Internet. But the code is stop at the while of adc flag. I don't know why it didn't work. If I delete the flag while. the adc value keep 0, it's not i want. I have no idea how to modify my code. And I use gnu tool to build the .bin file. Is it possible that I lose some important compile parameter?

this is me code. thx

uint32_t adcValue=0;

uint32_t adcVoltage=0;

int main()

{

init_adc();

ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_3Cycles);

while(1){

//Start ADC1 Conversion

ADC_SoftwareStartConv(ADC1);

while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

adcValue= ADC_GetConversionValue(ADC1);

adcVoltage = adcValue * (5.0/4096.0);

}

}

void init_adc()

{

ADC_InitTypeDef ADC_InitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

ADC_CommonInitTypeDef ADC_CommonInitStructure;

        //Enable ADC1 

RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

//Enable the ADC1 GPIO Clock

      RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); 

//Initializing GPIO for ADC

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_Init(GPIOC, &GPIO_InitStructure);

//ADC Common Init

//Use Independent mode

ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

ADC_CommonInit(&ADC_CommonInitStructure);

//ADC1 Init

ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

ADC_InitStructure.ADC_ScanConvMode = DISABLE;

ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStructure.ADC_NbrOfConversion = 1;

ADC_Init(ADC1, &ADC_InitStructure);

//Enabling Temperature sensor

ADC_TempSensorVrefintCmd(ENABLE);

//Enable ADC1

ADC_Cmd(ADC1, ENABLE);

}

#stm32f4-adc-battery
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on April 21, 2013 at 16:42

You're not using 5V as a reference voltage.

You're mixing float and integer math.

You're using the wrong channel. PC5 is channel 15

You should perhaps review the firmware examples more carefully,.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ctc.ctc
Associate II
Posted on April 21, 2013 at 17:54

thank you for your reply

but I try channel 15 to run adc

it still block at the flag loop =(