STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429I-DISCO USB FW Upgrade code issue

Posted on October 16, 2013 at 18:37STM32F429I-Discovery_FW_V1.0.0\Projects\FW_upgrade\src\usb_bsp.c PE1 (SDRAM NBL1) is NOT the over current pin, OTG_FS_OC is PC4 per the schematic #define HOST_OVRCURR_PORT                  GPIOE #define HOST_OVRCUR...

DAC offset problem

Posted on October 18, 2013 at 09:50HII have a small issue with the DAC in a stm32F103, there Is a small offset between DAC_DHR12R1 and DAC_DOR1 registersThe code is pretty simple:DAC_InitStructure.DAC_Trigger = DAC_Trigger_Software;DAC_InitStructure...

spa23 by Associate III
  • 991 Views
  • 2 replies
  • 0 kudos

STM32F2 GPIO glitch-free startup

Posted on October 23, 2013 at 01:51Are the GPIO of the STM32F2 guaranteed to be high-impedance, glitch-free during power ramp-up? #stm32f2-gpio-start-up-glitch

Endpoint problem.

Posted on October 30, 2011 at 08:01Hello,I have STM3210C-EVAL board. The HID mouse example is working well.But, if I change the endpoint from 0x81 to 0x82, it doesn't work.In addition, for TX2 buffer I changed buffer size to 128 like#define TX2_FIFO...

tonykwon by Associate
  • 1300 Views
  • 3 replies
  • 0 kudos

Stack Pointer Alignment ? (printf float problem)

Posted on October 22, 2013 at 17:30Hello,I am observing variables of my application with IAR Terminal I/O while debugging.But when trying to printf() float values, like; printf(''%f '', myFloat); Terminal I/O gives %f as output.After checking over i...

eraycanli by Associate II
  • 2039 Views
  • 4 replies
  • 0 kudos

Software Reset on STM32F417 - Doesn't Work?

Posted on October 21, 2013 at 22:53Hi All, I am working with the STM32F417. I am developing a bootloader and I need to generate a software reset. According to the Cortex-M4 programming manual (PM0214), you can generate a software reset by writing to...

kevin23 by Associate II
  • 3122 Views
  • 4 replies
  • 0 kudos

STM32F4 Discovery Integrated LIS302DL Interrupt

Posted on October 22, 2013 at 15:28Hi Everybody and thanks in advance for support.I'm trying to rewrite code to read LIS302DL to handle/generate an interrupt every Data Ready Signal.Here is my code RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE...

peppea82 by Associate II
  • 1252 Views
  • 2 replies
  • 0 kudos

how the image is sent to the camera to the computer?

Posted on August 12, 2013 at 10:32I have a project with OV7670 with stm32f4-discovery. My OV7670 has 16 pins and without fifo. I'm havinga picture ofthe camera and than I have to send my picture to the computer. But I have no idea how I'm gonna do. ...

DCD_DevDisconnect doesn't work

Posted on October 20, 2013 at 23:28I have a simple task, to cause a USB disconnection and reconnection when I boot my STM32F2.I tried using DCD_DevDisconnect after initializing the core (I am using the HS core, no DMA, not in OTG mode), but my USB a...