Question
6 CH PWM on TIM1 (What is Wrong with my Code)
Posted on February 06, 2013 at 11:09 Hello, I am currently migrating from Microchip MIP to ST ARM Cortex M3 so I am new to Cortex M3.I have been trying for days to configure Advance TIM1 in STM32F103RB to output 6 Channel PWM but it has prove to be a difficult task. When I probe PA8--PA10 using my Salae Logic Analyzer, there are no PWM on those Pins.. I have gone through my Code, Data sheet and App Note several times but I can not get it to Work. I do not want to use ST Peripheral Library. I prefer bare metal because it enable me to understand the Hardware.My Code is below and I desperately need help Note: CoCoox IDE and ARM GNU 4.7 C Compiler Used in building the Code. ===================== #include ''stm32f10x.h'' void PWM_init(void); int main(void) { volatile uint32_t dly; RCC-> CFGR |= RCC_CFGR_ADCPRE_DIV4; //ADC divided by 4 /*Enable all GPIO Clock & Alternate Function Clock*/ RCC->APB2ENR = RCC_APB2ENR_AFIOEN | RCC_APB2ENR_IOPAEN | RCC_APB2ENR_IOPBEN | RCC_APB2ENR_IOPCEN | RCC_APB2ENR_IOPDEN; /*Enable ADC1 & ADC2 Clock*/ RCC->APB2ENR |= RCC_APB2ENR_ADC1EN | RCC_APB2ENR_ADC2EN; /*Enable TIMER1 & USART1 Clock*/ RCC->APB2ENR |= RCC_APB2ENR_TIM1EN | RCC_APB2ENR_USART1EN; /*Enable TIMER2, TIMER3 & I2C1 Clock*/ RCC->APB1ENR = RCC_APB1ENR_TIM2EN | RCC_APB1ENR_TIM3EN |RCC_APB1ENR_I2C1EN | RCC_APB1ENR_TIM4EN; RCC->AHBENR = RCC_AHBENR_DMA1EN ; //DMA1 clock enable GPIOB->CRH = 0x44444222; //Configure PB8 & PB9 as Output (Push Pull) GPIOA->CRH = 0x44444AAA; //PA8 - PA10 Alternate Function Push Pull Output AFIO->MAPR |= AFIO_MAPR_USART1_REMAP; // Remap TX=>PB6, RX=>PB7) PWM_init(); //Initialize 20KHz PWM on CH 1-3 while(1) { for(dly = 0; dly < 500000; dly++); GPIOB->BSRR = (1 << 8); GPIOB->BSRR = (1 << 9); for(dly = 0; dly < 500000; dly++); GPIOB->BRR = (1 << 8); GPIOB->BRR = (1 << 9); } } /* PWM CH1=>PA8, PWM CH2=>PA9, PWM CH1=>PA10*/ void PWM_init() { /* channel 1&2 is configured as output*/ TIM1->CCMR1 &= ~(TIM_CCMR1_CC1S | TIM_CCMR1_CC2S); TIM1->CCMR2 &= ~(TIM_CCMR2_CC3S); //channel 3 is configured as output /* Channel 1,2& 3 active high */ TIM1->CCER = TIM_CCER_CC1P | TIM_CCER_CC2P | TIM_CCER_CC3P; TIM1->CCMR1 |= TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2; //PWM mode 1 TIM1->CCMR2 |= TIM_CCMR2_OC3M_2 | TIM_CCMR2_OC3M_1; //PWM mode 1 TIM1->CR1 = TIM_CR1_CMS_1 | TIM_CR1_ARPE; //Center-aligned mode 2 TIM1->CR2 = TIM_CR2_CCPC; //CCxE, CCxNE and OCxM bits are preloaded TIM1->BDTR = TIM_BDTR_MOE | TIM_BDTR_AOE | TIM_BDTR_OSSR; TIM1->PSC = 0; TIM1->ARR = 2800; // Auto reload value 2800 (PWM Period = 50us) TIM1->CCR1 = 1400; // Start PWM duty for channel 1 TIM1->CCR2 = 700; // Start PWM duty for channel 2 TIM1->CCR3 = 350; // Start PWM duty for channel 3 /* CH 1-3 Output Compare Enable*/ TIM1->CCER = TIM_CCER_CC1E | TIM_CCER_CC2E | TIM_CCER_CC3E; TIM1->CCER = TIM_CCER_CC1NE | TIM_CCER_CC2NE | TIM_CCER_CC3NE; TIM1->CR1 = TIM_CR1_CEN; // Counter enable } =================== Thanks Please Forgive my English