STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7B0 ULPI Timing in 1.8V and PHY Selection

I am currently working on using the USB3320 ULPI PHY with the STM32H7B0VBT6. After reading the STM32 reference manual, I noticed that it mentions special attention should be paid to the hold time when operating at 1.8V.Additionally, I came across a f...

屏幕截图 2024-11-08 035441.png
Cirno by Associate
  • 2149 Views
  • 2 replies
  • 2 kudos

Resolved! Stm32f105 don't enter dfu mode

Posted on November 05, 2012 at 11:29Hello, I designed a board which contains stm32f105 microcontroller, and i want to use DFU as bootloader in order to download my program to the micro controller through usb port. I put BOOT0 =1, and BOOT1=0 PA10=PD...

hisham23 by Associate III
  • 2050 Views
  • 2 replies
  • 1 kudos

Resolved! Cortex M7 Operating Modes

Hii, In ARM cortex M7 Architecture, Two modes are there one is Thread Mode and Handler Mode. Here, What is my query is How to switch Thread mode to Handler Mode? What Instruction we have to write example, msr xpsr in Assembly? Regards,

why calibration ADC and DAC is important in stm32f4?

  Hello, I am using ADC and DAC for sensing in my device, and I am using the STM32F405RGT6. I want to perform calibration, but I cannot use   "HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);"   . I tried using this code: c Copy code     ...

macam1 by Associate III
  • 9379 Views
  • 10 replies
  • 4 kudos

Resolved! Nucleo446re Internal Adc

Hi Everyone I am using Internal adc to sample 2 channels of adc using polling methodI am not able to reduce the number of samples per cycle by changing prescaler or Sampling timeI can only control the samples per cycle by giving software delay -->   ...

harry123 by Senior II
  • 1574 Views
  • 1 replies
  • 1 kudos

SD Card as MSC Device on STM32H753I-EVAL2

Hello everyone,I’m looking for some assistance with making an SD card work as a Mass Storage Class device on the STM32H753I-EVAL2 board. I’ve come across various solutions on the forum that have helped others, but none have resolved all the issues, a...

ikogman by Associate II
  • 2052 Views
  • 3 replies
  • 1 kudos

Resolved! USB not recognized by PC in FreeRTOS

Hi, I want to get log using Type-c, and using freertos to run all the tasks.setting:MCU STM32L4A6VGSTM32CubeIDE 1.12.0STM32CubeMX  6.8.0tera term 4.106when i insert Type-c, device manager return the unknown usb.I try some methods:1. put MX_USB_DEVICE...

alyssa_0-1723607387160.png alyssa_1-1723607401827.png alyssa_2-1723607423269.png alyssa_4-1723607858546.png
alyssa by Associate III
  • 10137 Views
  • 9 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.