STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RB DMA UART problem

Posted on January 10, 2014 at 10:46 Hi, I use STM32 vl-discovery in my project. I've connected and configured USART1 + DMA1 with informations and code from this forum. Application almost works, but all data in DMA memory receive buffer...

Discovery 32F3xxx Using USB to C# program on PC

Posted on January 10, 2014 at 14:38In general, how do I go about getting a program I write which runs on the Discovery board to communicate with a PC over one of the USB links? Anyone got a pointer to reference material or examples?Dirk

dbruere by Associate
  • 1693 Views
  • 4 replies
  • 0 kudos

stm32F4 sdio write multiblock problem

Posted on January 10, 2014 at 03:32when i try to write data into a file use SD_WriteMultiBlocks function then some blocks didnt fill the data i want, the block looks filled with old deleted file data and all this blocks start with XXXXXe00 end with ...

STM32F1 encoder problem

Posted on January 09, 2014 at 09:56I have a board with an STM32F100 and a quadrature encoder connected to TIM1 channels 1 and 2 PA8 and PA9, the index output is connected to GPIO pin. I have checked the input from the encoder and it is generating th...

STM32F105 Shared Pin PA9 (USART1-TX and VBUS) conflict

Posted on January 05, 2014 at 19:36Hello, the STM32F105 Device share USART1-TX and VBUS for USB on Port PA9. I need the USART1 for communication and for the internal Bootloader (only USART1 on my used 64pin Devices possible), if the firmware corrupt...

ralf by Associate
  • 1170 Views
  • 2 replies
  • 0 kudos

Interrupt priority problem

Posted on January 08, 2014 at 16:06HiI'm working on a project where I use a interrupt from the RTC. This is the one second interrupt. I also use a couple of other interrupts, for example timer 3. The RTC interrup can have the lowest interrupt possib...

m_ by Associate II
  • 3611 Views
  • 8 replies
  • 0 kudos

EXTI line 13 always pending? (STM32F103VG) Solved!

Posted on January 10, 2014 at 06:05Hello all, hopefully someone can see the error of my ways? I have a some hardware with a couple of rf modules IO lines connected to Port D pins 10, 11, 12, 13. All is well except for pin 13 which is always providin...

Help me choose a programmer [newbie]

Posted on January 08, 2014 at 21:05I have a legacy system that uses a STM32F103RE device and I would like to connect to it via JTAG (or any other on board option) and view the code on the device to verify it's version (and possibly update).  It seem...

STM32f-Discovery USART send BREAK

Posted on January 09, 2014 at 17:19I have setup the USART to Tx/Rx however my application requires sending a Break. The STM32F programmer's manual refernces sending Idle and Break, provides an example and register for sending an idle character but n...

vendor by Associate II
  • 2309 Views
  • 4 replies
  • 0 kudos