STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 USB Virtual COM problem

Posted on October 25, 2013 at 16:13Hi, I am using olimex kit of  STM32F103RBT6 microcontroller. I am new in USB virtual COM programming. I am using STM32_USB-FS-Device_Lib_V3.3.0 with Keil MDK-ARM 5.0 IDE. I opened the precompiled Virtual Com port p...

Measuring Vdd through Vbat

Posted on January 07, 2014 at 23:00Using an STM32F407xx, I want to monitor Vdd by connecting it to Vbat and using ADC1_IN18. If I am not actually powering my device from the battery, is it still possible (or advisable) to do this?The reason that I a...

dibs by Associate II
  • 4202 Views
  • 7 replies
  • 0 kudos

Hard Fault test error?

Posted on January 09, 2014 at 13:14In order to test the Hard Fault interrupt, I modified the Systick example on ''STM32F0xx_Discovery_FW_V1.0.0'' as follows.. on main.c I added two lines: ------------------------------ int main(void) { uint8_t* Byte...

How to calculate date,month and year ?

Posted on January 08, 2014 at 08:35Guys, How to calculate date,month and year ? from RTC_GetCounter function, I saw : uint32_t RTC_GetCounter(void) {   uint16_t tmp = 0;   tmp = RTC->CNTL;   return (((uint32_t)RTC->CNTH << 16 ) | tmp) ; } I've done ...

STM32L1xx performance question

Posted on January 04, 2014 at 13:57 Dear Sir/Madam, In the past I have been using 8-bit AVR (Atmega328p) for my application. The application uses the following peripherals: - I2C peripheral and - USART peripheral The ...

klemen by Associate II
  • 3436 Views
  • 9 replies
  • 0 kudos

Extra interrupts generated when using DMA and SPI?

Posted on January 07, 2014 at 02:03I have a STM32 discovery board configured in slave mode receiving commands over SPI. When it receives a specific command byte, it activates DMA and sends back a set number of bytes back. I have a print statement at...

Buffer sizes for SPI and DMA

Posted on January 06, 2014 at 18:27 Quick Question: I'm using DMA to transfer some data over SPI, and the first time round, I'm sending data from a buffer of size 3 bytes. I then redefine the DMA to try and send a buffer of size 4 bytes, but it ...

How to play wav on STM32F4 Discovery?

Posted on January 09, 2014 at 01:20Guys, How to play wav on STM32F4 Discovery? If I want to play from USB Key, I enable : #define MEDIA_USB_KEY and how to connect USB flash drive to this board ? with adaptor ? the socket is too small for USB flash d...