cancel
Showing results for 
Search instead for 
Did you mean: 

STMPE610 - Problem with Touch Detection

epetrou
Associate
Posted on May 22, 2013 at 16:47

Hi Forum users,

I try to bring in my project all the advantages that a TFT Display with touchscreen promises. The touchscreen controller STMPE610 with the Displaytech's TFT Display, DT028ATFT-TS, is used but unfortunately till now I cannot make it work.The Initialisation commands are sent with I2C and it seems that works fine.

According to the attached schematic ''TS-Controller_Circuit.JPG'', the IN2 and IN3 are not used and I connected them to the GND with a 10k resistor in between. The capacitors connected to the signal lines TFT_YU, TFT_YD, TFT_XR and TFT_XL are not 2pF but 2.2nF 0603. The interrupt signal TS_INT is connected to an MCU input (R8, pull-up resistor).

Now, getting to the point ... I have measured the following voltages with or without touching the surface

 Vio = 3.28V

 V_XL or V_X- = 3.27V

 V_XR or V_X+ = 0V

 V_YU or V_Y+ = 0V

 V_YD or V_Y- = 0V

and no interrupt is generated. What seems the problem? Probably is my misunderstanding of the controller, so pls could you tell me where I've got it all wrong???

Thanks a lot all of you, in advance!!!

P.S. This is the initialisation code

void STMPE610_Init(void)

{

    __delay_cycles(1000);

    

    //STMPE610_Write(SYS_CTRL2, 0x0F);     // Disable TSC and ADC Blocks

    //__delay_cycles(10);

    

//    STMPE610_Write(TSC_CTRL, 0x43);     // Enable Touchscreen, 32 points tracking index, X, Y mode

//    __delay_cycles(10);

//    STMPE610_Write(SYS_CTRL1, 0x02);    // Reset Device

//    __delay_cycles(100000);    

    

    STMPE610_Write(SYS_CTRL2, 0x0C);     // Enable TSC and ADC Blocks

    __delay_cycles(10);

    STMPE610_Write(INT_EN, 0x01);         // TOUCH_DETECT-Interrupt are enabled

    __delay_cycles(10);

    STMPE610_Write(ADC_CTRL1, 0x49);     // 80 clock cycles for ADC conversion, 12-bit ADC and internal ref

    __delay_cycles(10000);               // delay 2ms

    STMPE610_Write(ADC_CTRL2, 0x01);     // ADC Clock = 3.25 MHz

    __delay_cycles(10);

    STMPE610_Write(GPIO_AF, 0x00);

    __delay_cycles(10);

    STMPE610_Write(TSC_CFG, 0x9A);         // Average Control: 4 samples

                                         // Touch detect delay: 500us

                                         // Panel driver settling time: 500us

    __delay_cycles(10);

    STMPE610_Write(FIFO_TH, 0x01);         // Not zero value

    __delay_cycles(10);

    STMPE610_Write(FIFO_STA, 0x01);         // Clear the FIFO Memory Content

    __delay_cycles(10);

    STMPE610_Write(FIFO_STA, 0x00);         // FIFO back to operation mode

    __delay_cycles(10);

    STMPE610_Write(TSC_FRACT_XYZ, 0x07);// Data Format for Z-Value

    __delay_cycles(10);

    STMPE610_Write(TSC_I_DRIVE, 0x01);    // Choose 20mA driving channel

    __delay_cycles(10);

    STMPE610_Write(TSC_CTRL, 0x03);     // Enable Device, No tracking index, X, Y, Z mode

    __delay_cycles(10);

    STMPE610_Write(INT_STA, 0xFF);        // Clear all interrupt status

    __delay_cycles(10);

    STMPE610_Write(INT_CTRL, 0x03);     // Enable the interrupts

    __delay_cycles(10);

    

    // define initial Touch Window

    /*STMPE610_Write(WDW_TR_X, 0x0FFF);    // Top Right X

    __delay_cycles(10);

    STMPE610_Write(WDW_TR_Y, 0x0FFF);   // Top Right Y

    __delay_cycles(10);

    STMPE610_Write(WDW_BL_X, 0x0000);    // Bottom Left X

    __delay_cycles(10);

    STMPE610_Write(WDW_BL_Y, 0x0000);   // Bottom Left Y

    */

}
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
epetrou
Associate
Posted on May 24, 2013 at 08:40

Hi all,

the problem is solved. A pin of the FPC connector was not correctly soldered. The circuit works with 2.2nF or 2pF capacitors. This is the initialisation code that I used

void STMPE610_Init(void)

{

__delay_cycles(1000);

STMPE610_Write(SYS_CTRL2, 0x0C); // Enable TSC and ADC Blocks

__delay_cycles(10);

STMPE610_Write(INT_EN, 0x01); // TOUCH_DETECT-Interrupt are enabled

__delay_cycles(10);

STMPE610_Write(ADC_CTRL1, 0x49); // 80 clock cycles for ADC conversion, 12-bit ADC and internal ref

__delay_cycles(10000); // delay 2ms

STMPE610_Write(ADC_CTRL2, 0x01); // ADC Clock = 3.25 MHz

__delay_cycles(10);

STMPE610_Write(GPIO_AF, 0x00);

__delay_cycles(10);

STMPE610_Write(TSC_CFG, 0x9A); // Average Control: 4 samples

// Touch detect delay: 500us

// Panel driver settling time: 500us

__delay_cycles(10);

STMPE610_Write(FIFO_TH, 0x01); // Not zero value

__delay_cycles(10);

STMPE610_Write(FIFO_STA, 0x01); // Clear the FIFO Memory Content

__delay_cycles(10);

STMPE610_Write(FIFO_STA, 0x00); // FIFO back to operation mode

__delay_cycles(10);

STMPE610_Write(TSC_FRACT_XYZ, 0x07);// Data Format for Z-Value

__delay_cycles(10);

STMPE610_Write(TSC_I_DRIVE, 0x00); // Choose 20mA driving channel

__delay_cycles(10);

STMPE610_Write(TSC_CTRL, 0x03); // Enable Device, No tracking index, X, Y, Z mode

__delay_cycles(10);

STMPE610_Write(INT_STA, 0xFF); // Clear all interrupt status

__delay_cycles(10);

STMPE610_Write(INT_CTRL, 0x03); // Enable the interrupts

__delay_cycles(10);

// define initial Touch Window

STMPE610_Write(WDW_TR_X, 0x0FFF); // Top Right X

__delay_cycles(10);

STMPE610_Write(WDW_TR_Y, 0x0FFF); // Top Right Y

__delay_cycles(10);

STMPE610_Write(WDW_BL_X, 0x0000); // Bottom Left X

__delay_cycles(10);

STMPE610_Write(WDW_BL_Y, 0x0000); // Bottom Left Y

}

Have a nice day!!!