User Activity

Posted on August 13, 2014 at 00:06Hello.I'm following the procedure in AN2604 and trying to use an internal timer to measure the rtc frequency by looping back the rtc into a timer pin, in my case PA8 (Timer 1 channel 1), and then using PWM input cap...
Posted on April 29, 2014 at 19:11Hello.Using stm32f107 here.I've been using the v2.1.0 stm32 usb host device library to build a cdc device. I used the vcp example and modified it, but I'm seeing cases where a 64 packet is being lost.I think I may ha...
Posted on May 23, 2013 at 12:31https://cmsis.arm.com/vendor/stmicroelectronics/ has the SVD that describes processor registers but it appears to be missing important things like the system control block that contains all of the fault information reg...
Posted on May 10, 2013 at 20:58The latest released version of the standalone stm32 standard peripheral library is v3.5.0 but the version inside of the usb device driver download is v3.6.1. This has a handful of useful bug fixes.ST, are there plans t...
Posted on April 02, 2013 at 02:13Hello.I've gone through the process of selecting part values for a few other dc/dc converters but I'm stumped with the steps to do so for the MC34063. I'm starting with 12V and converting to 5V and 3.3v so I just cop...