STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM: drive output low in disabled mode

Posted on April 15, 2014 at 16:26I'm using TIM1 for a 6-step motor control on a STM32F2xx. According of the table 4 in DM0004234 application note, I update OCxE and OCxNE at each commutation, to select a new step. When OCxE = 0 and OCxNE = 0, the ou...

stinguely by Associate II
  • 3696 Views
  • 8 replies
  • 0 kudos

First Printf, some problems :-(

Posted on April 12, 2014 at 10:37The original post was too long to process during our migration. Please click on the attachment to read the original post.

DS1307 and STM32 ?

Posted on April 15, 2014 at 12:15Guys Does anyone of you have experience using DS1307 with STM32 ? Any links / references ? Thank

Some Problems with triple Channel ADC -- STM32f4

Posted on April 11, 2014 at 14:46Hello Together,I have a problem with my ADC. I tried to search through the Forum but I couldn't find a similar problem.My plan is to read 6 different Analog Digital Channel on STM32F407 therefore I use ADC1, ADC2 and...

breibold by Associate II
  • 3958 Views
  • 5 replies
  • 0 kudos

data transfer speeds

Posted on April 14, 2014 at 21:23Hi all, i'm dissapointed from transfer speeds on STM32F407 @ 168MHz core, i'm measuring roughly 10.7MHz using FSMC with the code: runTIM_stoptime();do{  hh=fsmc_read( 0 );}while( (ui32--) > 0 );stopTIM_stoptime();USA...

Cortex-A chips for Generating Pulses?

Posted on April 14, 2014 at 11:33I am now using a Cortext-M3 chip(STM32F) to control Stepping Motor in an industrial equipment (Only generating pulses and direction signal to send to a stepper driver). Its maximum frequency is 72MHz so I can't add m...

SWD Interface for STM32F051 and / or STM32F030

Posted on April 15, 2014 at 01:51I have a STM32F030 design which I migrated from a STM32F051 design.  When I read documentation on the programming interface, it specifies SWDCLK, SWDDIO, and NRST.  I noticed however that the Discovery board has anot...

mvonahnen by Associate III
  • 1200 Views
  • 3 replies
  • 0 kudos

BT.656 to RGB

Posted on April 03, 2014 at 16:26Hello guys, I've started reading about STM32F429 and start thinking -  if it would be possible to use LCD-TFT controller in such situation:microcontroller reads BT.656 video signal (8 or 10 bits in parallel + CLK), d...

Disabling USB

Posted on April 14, 2014 at 13:08Does anyone know the easiest way to disable USB? I have a bootloader which makes use of the usbh to download a program from a usb flash drive to flash and then runs the program. The program also makes use of usb thou...