User Activity

Posted on February 11, 2016 at 00:23Hello,I have been tackling a USB issue on the STM32F373VC.My setup consists of a STM32F373 mcu setup  as USB Virtual COM port. On the host side, commands are sent from a PC(windows7, 64 bit) via a teraterm script....
Posted on March 28, 2014 at 00:34 Hello, I'm evaluating STM32cube, to see how it performs. I have a simple project in IAR which I created in STM32Cube for the F407 discovery kit. Enable PortD.12 and D/13 as outputs. However when I in...
Posted on July 26, 2013 at 22:15Sorry had to do this, but this is a request for Clive. There is no PM capability on these forums. If possible, Clive, could you please drop me a mail at admin AT 43oh.com I'd be grateful if you do. This does not rela...