STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-Link and the STM32F4 Discovery

Posted on February 06, 2014 at 01:21Hi Everyone,Sorry if this is a repeat post, I'm pretty sure I've looked through all of the past discussions related to this and still have not found a solution.I designed a new board using the STM32F427 and have b...

gabriel by Associate
  • 5217 Views
  • 11 replies
  • 0 kudos

Stm32100 lcd.c in STM32F10x_stdperiph_LIb hx8312 and hx8369

Posted on April 22, 2014 at 04:17Dear all, I found in the STM32F10x_stdperiph_LIb  file Stm32100_eval_lcd.c. This file is firmware driver for an LCD TFT with Hx8312 Controller. I want to use an LCD TFT of Newhaven Display with Hx8369 Controller (an ...

btiendat by Associate
  • 2686 Views
  • 1 replies
  • 0 kudos

Speex Library

Posted on April 22, 2014 at 16:19Hi all, I'm trying to use the speex library on a STMF205. I have downloaded the AN2812 and the stsw-stm32017 example. I have copied code example into  my project  :     /* Speex encoding initializations */     speex...

dbouvier by Associate II
  • 1442 Views
  • 2 replies
  • 0 kudos

STM32F407VGT6 - ADC pins unused ?(VREF+,VREF-,VDDA,VSSA)

Posted on April 03, 2014 at 17:45Hello everyone, i am trying to design a board around STM32F407VGT6 and i want to use minimum components. i will not use the ADC for any purpose , is it possible to leave the pins related to it (VREF+,VREF-,VDDA,VSSA)...

testid360 by Associate II
  • 3372 Views
  • 5 replies
  • 0 kudos

C++ relevant bug in generated usbd_conf.h

Posted on April 15, 2014 at 22:08I found out that in my case the generated usbd_conf.h file contains a bug which is only visible when including it from a c++ file. The code contains the typical conditional 'extern ''C''' declaration at the beginning...

henry by Associate
  • 975 Views
  • 1 replies
  • 0 kudos

IAP programming errors

Posted on April 01, 2014 at 15:06 Dear List, I am working on IAP on the STM32F4Discovery board and flashing only occasionally works. I started from the example describing IAP using an USART. But I use USB to download the data...

Sietse by Associate III
  • 5466 Views
  • 14 replies
  • 0 kudos

No VBAT pin on STM32L152 ?

Posted on April 14, 2014 at 18:48Hi All,Can anyone please advise why there is no VBAT pin on STM32L152 MCU?I read that RTC runs as long as the MCU is powered...but when its not, then what ?How to implement RTC backup supply on this MCU?Thanks!regard...

Tom by Associate II
  • 2464 Views
  • 5 replies
  • 0 kudos

STiH207 ?

Posted on April 21, 2014 at 09:15Guys, STiH207I'm just wondering, where can I find the discussion for this chip ? thanks https://my.st.com/st-extranet-web-active/active/en/catalog/mmc/FM131/SC999/SS1629/PF252588Guys, STiH207Advanced dual HD AVC proc...

SDHC and SDXC ?

Posted on April 20, 2014 at 05:22Guys, I tried to read SDHC 8Gb with SDIO and it works fine, but when I change into 64Gb SDXC, it doesn't work ? Do you have any ideas what the cause is ? When I tried with SPI and Atmega controller and SPI , they're ...

Microcontroller load

Posted on April 21, 2014 at 11:17How do I calculate/decide the clock frequency of a microcontroller and load it can take?for example, if a controller is capable of 32MHz clock frequency, with 4UARTs, USB host, 2 I2C & SPI, 20 GPIOs, an LCD controlle...