Posted on August 10, 2013 at 01:41Can anyone help me with the problem below dotted line? It seems like I need to set up memory spaces for the Micro Controller. Is that ? the problem. If so how do I fix? Thanks! GDN -------------------------------...
Posted on August 07, 2013 at 23:41I have a STM32 Discovery Kit. I have set up the IAR compiler. Succesfully compiled code. However when I try to download the the Discovery Board I get the following message... Wed Aug 07, 2013 14:21:48: Fatal erro...
Posted on August 08, 2013 at 21:24Clive, OK this turned out to be pretty simple! There are two thing that need to be done in the IAR to allow you to configure to the ST-Link. Under Options->Debugger->Driver...Select ST-Link Under Options->ST-Link...