STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Inputs GPIO

Posted on May 09, 2014 at 22:09Hello everybody.I want to solve a read problem in a special hardware, the configuration of each pin is input:RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GP...

Question about the mass erase feature

Posted on May 09, 2014 at 19:14I have been reading the ''PM0075'' Programing manual STM32F10xxx Flash memory micro-controllers and I am trying to understand the mass erase feature.  In the manual it states:''Bit 2 MER: Mass eraseErase of all user pa...

ebommer by Associate II
  • 883 Views
  • 1 replies
  • 0 kudos

SWO output on IAR Demo Project

Posted on April 29, 2014 at 20:24I'm working on the STM32F439-EVAL. I've created my own project using STM32Cube and am able to use SWO output and see the logs on the IAR terminal IO window (I'm using IAR). In order to compare some of the bootup proc...

kartik by Associate II
  • 1742 Views
  • 2 replies
  • 0 kudos

STM32f303 Output Compare

Posted on May 09, 2014 at 15:48Hello, i'd like to do output compare on four pins: PE13, PE9 (LEDS), PA10 and PA12. Everyone works except PA12. I tried to do that with TIM16 and TIM4 with no luck. And i reconfigured the channels, i understand how the...

arganasss by Associate II
  • 1555 Views
  • 3 replies
  • 0 kudos

STM32F401VE: No library support for SPI4?

Posted on May 09, 2014 at 14:34I have been looking in the stdlib libraries (v 1.0.2) for the STM32F401VE, and there does not seem to be any support for SPI4, even though it is listed as existing in the datasheet and reference manual. What gives?Have...

dibs by Associate II
  • 1326 Views
  • 2 replies
  • 0 kudos

ST MDK5 CMSIS device driver packs examples

Posted on May 09, 2014 at 15:48Hi, Has anyone started using V1.0.7 Keil.STM32F4xx_DFP.1.0.7.pack? We are considering  to use it as a part of medical product development. I also do not see any example codes as a part of this pack (particularly requir...

vasanth by Associate
  • 680 Views
  • 0 replies
  • 0 kudos

STM32F0 ADC Temperature Drift?

Posted on May 08, 2014 at 17:48Simple question - should be answered in datasheet, errata sheet, or ref manual but I cannot seem to find it. I am wondering how much ADC readings drift relative to the reference voltage with temperature. If I have a co...

Tutorials, etc.

Posted on May 06, 2014 at 07:17Is there a tutorial or lecture series for beginners working with a STM32F3 demo board? I have programmed simple project boards like Arduino, but not anything like the STM32 boards. I have tried to work backwards from t...

jprevard by Associate II
  • 5018 Views
  • 11 replies
  • 0 kudos

stm32f405, lock question

Posted on May 06, 2014 at 00:33Dear, i have the following issue: i have seen that i cannot process too many instructions from inside interrupt. I guess there is a limit. (still didn't looked the datasheet), So i decided to do just some few operatio...

Angelo1 by Associate II
  • 2963 Views
  • 7 replies
  • 0 kudos

STM32F205ZGT6 - PC13 as output doesn't work

Posted on May 08, 2014 at 20:36 Hello, I'm trying to use the PC13 as an output but I can't get any signal change from it. I'm already setting the pins PC14 and PC15 as inputs following the datasheet orientations. I used one of the ...

gui by Associate
  • 996 Views
  • 1 replies
  • 0 kudos