cancel
Showing results for 
Search instead for 
Did you mean: 

Bypass capacitors for STM32F0 series?

jksystem247
Associate II
Posted on October 09, 2013 at 10:43

Hi.

I am designing a test board using STM32F0 series MCU.

On the datasheet, it states I have to attach 3 bypass capacitors(2 x 0.1uF, 1 x  4.7 uF) per each VDD. 

Is it absolutely necessary?, What is the point of using two identical capacitor, when I can use a single capacitor with about 0.2uF value? so that I only have to use 2 capacitors per each VDD pin saving me the board real-estate?

Anyone have ideas??

Thank you.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cpinkstone2
Associate II
Posted on October 09, 2013 at 10:53

Hello188

You've just misread it. It's one 0.1uF per Vdd pin (local de-coupling) and a single 4.7uF for the chip as a whole.

jksystem247
Associate II
Posted on October 09, 2013 at 11:09

Thank you so much!!