cancel
Showing results for 
Search instead for 
Did you mean: 

stm32L discovery onboard st-link

kkkuba
Associate II
Posted on October 06, 2013 at 23:12

Hi,

I've got a question about using ST-LINK/V2 to program/debug an external application:

if onboard st-link can be used only for MCUs from STM32L1 series or from other series too?

I'm asking because in UM1079 it is written (quote) ''Using the ST-LINK/V2 to program/debug an external STM32L application'', so I want to know if this is a restriction on series of MCU
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on October 07, 2013 at 06:31

That must be an unintended typo. The STLink there is a generic one. Incidentally, I currently use a ''L DISCOVERY'''s STLink to develop on F4...

JW

kkkuba
Associate II
Posted on October 07, 2013 at 13:28

thanks for reply

regards

Posted on October 07, 2013 at 18:07

Make sure to use the most current firmwares to support the newest devices. I'm not sure ST has released the most current ones, the update on Keil is newer (V2.J16.S0) than one with ST-Link Utilities (V2.J15.S0), and I've seen V2.J17.S0 on the STM32F401C-DISCO board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..