STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

emmc interfacing with NUCLEO board

I’m interfacing the STM32H755ZI-Q Nucleo board with an MTFC8GAMALNA-AAT eMMC. What configurations are necessary for this interfacing? I’m also getting warnings in the RCC configurations. Could you guide me on the settings needed for SDMMC1 and FATFS,...

sai1 by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

Resolved! Questions about SPI6 and BDMA

We are trying to transmit data using SPI6 and BDMA.When we perform the following process, we are able to transmit 1 byte + 1 bit of data, but after that, MISO outputs High no matter what the value of the transmitted data is. What is wrong with this? ...

Resolved! Ext. Interrupt conflict on STM32H7 ?

Hello, I'm using H723 Nucleo. I set 5 ext interrupt pins: PA0, PA1, PA4, PC2_C, and PC13 as EXTI to 5 switches, enabled NVIC interrupt, GPIO pull-up,  interrupt with rising edge triggered, and tied these 5 pins to switches with the other end to groun...

DSIHOST_D1P pin used as GPIO

Hello,I'm wondering if there's a way to use the DSIHOST_D1P and D1N pins as GPIOs, or if it's possible to simulate GPIO functionality on these pins. Currently, I don't see any GPIO configuration options for them in STM32CubeMX. The MCU in use is the ...

Resolved! SPI CR1 bit SPE will not set

I am writing my own SPI driver, and using two B-L072Z-LRWAN1 boards to test them; one as an SPI master and one as a slave. On the master device, whenever I enable the SPE bit in the function SPI_Transmit(), it never actually sets to '1', even though ...

STM32H5 support for MX25L6433F

Hello Everyone,Is there any plan for ST to provide support drivers for the MX25L6433F serial NOR flash on the STM32H5 series of micros?MX25L6433F is the flash used on the X-NUCLEO-GFX01M2.Thanks.