STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Config i2c with no external pullups

Posted on May 15, 2014 at 15:46I'm trying to connect my STM32F100 Discovery board to a sensor using the I2C bus. The sensor resides on a breakout board and I am using clip leads to go from my Discovery board to the breakout board. How would I config...

saccrue by Associate II
  • 1816 Views
  • 4 replies
  • 0 kudos

stm32f107vc (olimex stm32-p107 revB) usart2

Posted on May 13, 2014 at 17:03 Hi all, As I have basically spent the whole day on this problem, trying to figure it out by myself, I am hoping to get some help from someone more experienced. My setup is the following: -(olimex s...

hagen by Associate
  • 1619 Views
  • 3 replies
  • 0 kudos

Bootloader and jumping to flash location

Posted on March 13, 2014 at 16:18 Hi guys, I've been working on a bootloader program which is loosely based around the FW_Upgrade demo for the STM32F4 discovery board. My Bootloader so far correctly finds a file on a USB stick and downloa...

DMA SDIO TX underrun error

Posted on March 08, 2014 at 14:46I got the DMA working fine with SDIO , i can read multiple blocks ok , but when i try write multiple blocks , i get TX underrun error in the SDIO , and i can also see that there is a FIFO error in the DMA , which i d...

STM32F103 USART (overrun)

Posted on May 14, 2014 at 16:18 Hello, I am using USART 1 at 115200 and todayserious problems with USART overrun started to appear (yesterday everything was fine and I don't seem to remember any significant changes on this portion of the ...

oversc0re by Associate II
  • 3074 Views
  • 4 replies
  • 0 kudos

ACD1_In16 configuration

Posted on May 14, 2014 at 19:40I'm having some trouble configuring this ADC, I need to read the temperature of the internal sensor from the STM32F3 Discovery. But in order to do so I have to configure this particular ADC (ADC1_in16)

STM32 VDE self-test library for stdperiph_lib

Posted on May 08, 2014 at 09:28Dear ST; I want to Optimize my program,so for the safety,I need the self-test library.but I can not find it on the st.com,so I come here to get help from you guys. Thanks very much. Yours, liuwei #stm32f10x #stm32 #...

994724682 by Associate II
  • 3219 Views
  • 8 replies
  • 0 kudos