STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switch statement error

Posted on May 15, 2014 at 18:09Hi I just can't understand this... So, I'm communicating with PC's terminal program via USART2 on my STM32F10. Communication is running smoothly both ways, but I have a problem when I want my embedded system to respond...

0690X00000605YMQAY.png
codium by Associate II
  • 4892 Views
  • 8 replies
  • 0 kudos

Interrupts and loss of Data

Posted on May 15, 2014 at 19:35I am currently building a big project on STM32F4 Discovery board for my graduation project. I have configured 4 Timers' interrupts (10Hz, 50Hz, 100Hz and 1kHz), USART communication with interrupt, and CAN communication...

mejrissi by Associate II
  • 4456 Views
  • 9 replies
  • 0 kudos

RTC Flags problem when alarm is set

Posted on May 16, 2014 at 13:37 Hi, My RTC (F103) is currently running from LSI. The counter is counting properly, and the SEC flag in CRL is set every second as expected. When the Alarm is set, the SEC flag is asserted and cannot be c...

STM32F05x SPI clk single bit

Posted on May 14, 2014 at 17:07 Hi, I have a PCB with a STM32F051 connected to 3 ADCs ( http://datasheets.maximintegrated.com/en/ds/MAX11166-MAX11pdf) in daisy chain. Page 29 Figure 14 of the datasheetshows the schematic I implement...

aoleon by Associate II
  • 2763 Views
  • 4 replies
  • 0 kudos

usb library on windows 7 (does not work)

Posted on May 01, 2014 at 18:46I am trying to use the usb library found here:  http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882#I am on windows 7, I am using the port207z board here with the STM32f207z: http://www.wvshare.com/p...

epataky by Associate II
  • 1584 Views
  • 4 replies
  • 0 kudos

Problem with USART1 Interrupt

Posted on May 15, 2014 at 15:13Hi all.I have a problem with USART1 Interrupt.Actually, I use usart1 to receive data from my PC via terminal. But I didn't receive any data.Could u show me the problem in my program.P/s: I use led 7 segments to view re...

huonglq91 by Associate II
  • 2618 Views
  • 6 replies
  • 0 kudos

ADC result alignment

Posted on May 16, 2014 at 04:05 Hello, I have problem to get the ADC alignment feature working. config: STM32F407 on discovery board, Adjustable voltage (0 to 3V) connected to PA3 ADC resolution set to 12b Whatever alignmen...

STM32 development board for motor driver

Posted on May 10, 2014 at 11:18Hi friends,               i am new to STM32 , and i want to design a motor driver of my own (i.e BLDC). can anybody tell me which development board will suit for this, and i have also attached the motor specification k...

ADC+DMA Start with Timer delay -Help needed!-

Posted on May 13, 2014 at 22:53 hello All, i want to start an ADC with DMA in a timer(5) interrupt routine. when i test timer and adc individually they work right. but when i insert ADC start, in timer isr the timer and adc works once and the...