STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST Link Utility v3.4 ?

Posted on May 13, 2014 at 11:31Hi All, I'm interested in the feature detailed in the v3.4 changelist which allows probe selection if multiple probes are connected, but the only version for download appears to be 3.3. Any clues as to the location of ...

jamie23 by Associate II
  • 2060 Views
  • 5 replies
  • 0 kudos

Crystal stops oscillating when debugging

Posted on May 09, 2014 at 03:22Hi, I have a board with an STM32F429 and an 8 MHz crystal on the HSE pins. I'm using Atollic TrueSTUDIO to upload and debug code. I can upload code without a problem, but as soon as the the debugger starts, the crystal...

STM32F4 (F4 discovery board) interrupt Issue

Posted on May 19, 2014 at 15:14Hi everybody, I have an unstable behavior on an ADC interrupt.My user code is very simple, I initialize my different peripherals (timer, ADC, GPIO) then I just a have an infinite  loop.My Callback for my ADC interrupt ...

Multiple pins with same function?

Posted on May 21, 2014 at 03:52Browsing through the STM32 F405 datasheet, I'm noticing serial ports with functions listed multiple times even on the same chip. At first I assumed (for example, USART1 TX) would be listed multiple times, but on any gi...

skeezix by Associate II
  • 10014 Views
  • 1 replies
  • 0 kudos

STM32F303CC not working

Posted on May 18, 2014 at 22:43Hi,I used the stm32f3 discovery board to test some code and it works fine but when I run the same code on a custom breakout I made around the stm32f303cc it runs for a while and then stops.The time it takes for the boa...

cbhar by Associate II
  • 5157 Views
  • 12 replies
  • 0 kudos

STM32 - discovery : ADC reference Voltage ?

Posted on May 20, 2014 at 16:46Hello,I am trying to get the reference voltage value with ADC (Channel 18).On the VCT6 datasheet, it is said that reference calibration values (for VREF) are stored in memory at the address 0x1FFFF7BA. (Value for VREF ...

thomas23 by Associate II
  • 1508 Views
  • 2 replies
  • 0 kudos

STM32F4xx alternate configuration SPI1 issues

Posted on May 19, 2014 at 14:04Hello Everyone,I was just wondering if anyone has seen this, I have seen this only referenced on one website.  I have SPI1 on a STM32F415 configured as   PA7   ------> SPI1_MOSI  PB3   ------> SPI1_SCK  PB4   ------> S...

gvigelet2 by Associate II
  • 5818 Views
  • 14 replies
  • 0 kudos

SPI Rx via DMA... SCLK generation?

Posted on May 19, 2014 at 21:41I'm wanting to update a product that has a SPI device on the same channel as the UART.  Currently the SPI device uses DMA - it sends 1 byte and receives a packet of info.  On the UART we only send data.I would like to ...

mreed by Associate III
  • 1802 Views
  • 4 replies
  • 0 kudos