cancel
Showing results for 
Search instead for 
Did you mean: 

STM Studio Variables missing

werbung
Associate II
Posted on January 15, 2014 at 22:55

Im using STM Studio 3.3.

When I import my .elf files from Keil or Coocox most of the variables (even direct variables) are missing.

When I analyze the .elf file with nm or eu-nm all the variables are available on fix RAM-adresses and I can manually add these adresses to the read or write list.

What is wrong with importing the .elf files in STM Studio ?

#stm-studio
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on January 24, 2014 at 11:51

Hi Henry,

Would it be possible to attach your .elf file for check? What are types of missing variables?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.