STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32f4-Discovery] I2S RX Master with DMA

Posted on March 06, 2013 at 19:44 Hi I have some questions for the following scenario. I want to configure the dma controller to transfer data from an digital i2s mems microphone to the memory. The I2S (SPI2) is the rx master and the memor...

Set USART2_RTS when GPIO is in alternate function mode.

Posted on August 25, 2014 at 16:06I have a STM32L152RCT6 mcu and a bluetooth module connected to usart2. I've also set up the dma for the communication. The gpio is set to alternate function mode. It works, however sometimes a packet loss happens. T...

zoltan by Associate
  • 1158 Views
  • 2 replies
  • 0 kudos

choosing pwm channel stm32f407 discovery board

Posted on August 23, 2014 at 11:29hi everybodyi want to have 8 channel pwm input and 8 channel pwm output in stm32f407vgt6here is the table of timers in this micro . i also want to have a time scheduling .from your perspective which combination of t...

0690X00000605QPQAY.png 0690X00000605NLQAY.png

STM32F205 DMA Problem

Posted on August 25, 2014 at 09:18Hello,I am trying to use DMA to transfer data from a buffer in RAM to a GPIO BSRR port triggered by a timer.  Due to the way the hardware is laid out I am committed to using TIM5 as the trigger.  The DMA trigger is ...

STM32 Cube and EXTI

Posted on August 25, 2014 at 08:23Containsorwill bein the next releaseincludesupportforSTM32CubeconfigurationEXTI? For exmple for STM32F0 and mappadle GPIO on external interrupt vectors.

a1379109 by Associate
  • 938 Views
  • 2 replies
  • 0 kudos