User Activity

Posted on September 23, 2014 at 08:28Hi, I'm currently running a STM32F4 Discovery board, connected to a AD1938 Codec. The STM32 is running as I2S Transmit Slave, with the clocks for WS(LRCLK) and BCLK coming from the AD1938. The STM32F4 is using th...
Posted on February 08, 2014 at 20:52I'm currently testing  I2S between two F4 Discovery development boards.One board is master, running DMA, one is slave. Both are configured with the same sample set for verification purposes, so the data sent can b...
Posted on January 11, 2014 at 10:45Hello,I've been spending some time looking through the STM32F4 reference document and it looks quite clear that the I2S2 / I2S2ext are supposed to be used in a full-duplex configuration.However, I'm curious, is it ...