2014-02-16 12:24 PM
Hello Based on some examples on the forum, here (Thank you).
I am using the STM32F407 based discovery board. I have the following code that works fine, but PA2, PA3, and PC4 do not give me the correct readings. As a test all Ain are connected to 1/2 VDD so the 12 bit response should be 0x0800 but for some reason they are being driven by something else. Right now I get 07FB080406DB0616080208010800080106DF07FD PA0 PA1PA2PA3PB0PB1PC1PC2PC4PC5 So my values for PA2, PA3, and PC4 are wrong and I can scope signals on PA2.volatile uint16_t ADCValues[10];
#define PORTA_ADCPORT GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3
#define PORTB_ADCPORT GPIO_Pin_0 | GPIO_Pin_1
#define PORTC_ADCPORT GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_5
/**************************************************************************************/
void RCC_Configuration(void)
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIOA_InitStructure;
GPIO_InitTypeDef GPIOB_InitStructure;
GPIO_InitTypeDef GPIOC_InitStructure;
GPIO_StructInit(&GPIOA_InitStructure);
GPIOA_InitStructure.GPIO_Pin = PORTA_ADCPORT;
GPIOA_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIOA_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIOA_InitStructure);
GPIOB_InitStructure.GPIO_Pin = PORTB_ADCPORT;
GPIOB_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIOB_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOB, &GPIOB_InitStructure);
GPIOC_InitStructure.GPIO_Pin = PORTC_ADCPORT;
GPIOC_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIOC_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOC, &GPIOC_InitStructure);
}
void ADC1_Configuration(void)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable peripheral clocks *************************************************/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* DMA2_Stream0 channel0 configuration **************************************/
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCValues[0];
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 10;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC1 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 10;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel configuration ******************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_480Cycles); // PA0
ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2, ADC_SampleTime_480Cycles); // PA1
ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 3, ADC_SampleTime_480Cycles); // PA2
ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 4, ADC_SampleTime_480Cycles); // PA3
ADC_RegularChannelConfig(ADC1, ADC_Channel_8, 5, ADC_SampleTime_480Cycles); // PB0
ADC_RegularChannelConfig(ADC1, ADC_Channel_9, 6, ADC_SampleTime_480Cycles); // PB1
ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 7, ADC_SampleTime_480Cycles); // PC1
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 8, ADC_SampleTime_480Cycles); // PC2
ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 9, ADC_SampleTime_480Cycles); // PC4
ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 10, ADC_SampleTime_480Cycles); // PC5
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 **************************************************************/
ADC_Cmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
}
void ReadADC(void)
{
puts(''ADC Testing\r\n'');
while (!(rxready()))
{
if (ADCValues[9] != 0xFFFF)
{
for (int loop = 0; loop < 10; loop++)
{
printf(''%04X '', ADCValues[loop]);
}
printf(''\r\n'');
ADCValues[9] = 0xFFFF;
}
}
}
2014-02-16 7:50 PM
Hello All,
So PA2 and PA3, were my dumb mistake. (was using them as SCI). And it turns out I didn't assign PC4. So everything works as it should, Thanks for the great examples people.2014-02-17 5:50 AM
So everything works as it should, Thanks for the great examples people.
That's good, I hadn't seen clashes on the pins in question.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.