Question
External SRAM interface problem
Posted on February 15, 2014 at 11:46
I got IS62WV12816BLL 128K * 16 bit SRAM to interface with STM32F207ZG , the problem is that i can not write properly to the SRAM , when i write say a word , i find that many addresses are written and only half the word is written correctly ...... i also see the value of the SRAM content changing as im moving to other breakpoints in the debug session ...... any suggestions ?