2014-02-15 3:15 AM
hi,
I have used STM32F417 processor with PSRAM 64 MB size and OV5640 Camera. I want to send the camera data from dma to PSRAM then PSRAM to UART4. How to configure the DMA for this above concept. Present dma settings uint8_t frame_buffer[640*480*2]; DMA_InitStructure.DMA_Channel = DMA_Channel_1; // DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(DCMI_BASE + 0x28); //vv added DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(DCMI_BASE); //vv added 0x50050000 // DMA_InitStructure.DMA_Memory0BaseAddr = FSMC_LCD_ADDRESS; //vv DMA_InitStructure.DMA_Memory0BaseAddr= (uint32_t)frame_buffer; //vv added DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; /* //DMA DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToMemory; */ // DMA_InitStructure.DMA_BufferSize=frame_buffer; DMA_InitStructure.DMA_BufferSize = 0x25800; //(640*480*2)/4 DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; //DMA_Mode_Normal Note:vv check this mode 0r DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; how to link DMA_PeripheralBaseAddr to PSRAM link,and i want to capture images snapshot 10 ms intervals and store this images to psram and send images one by one PSRAM to uart4. PSRAM Chip select address is FSMC_Bank1_NORSRAM2. my requirements is camera datas need to send via uart ,how to configure this Data flow for following method. DMA to PSRAM and PSRAM to UART4. Thanks by, Venkat2014-02-15 5:55 AM
Observations:
This is TWO separate tasks, you'll need to configure a separate DMA task for each. The USART being significantly slower. You need your buffer to be placed in your external memory. You need the DMA to increment that memory address. The DCMI data should come from &DCMI->DR, as I recall, and Half Words The longest DMA transfer is 65535 units The DMA for the UART4 will come from memory and go to the UART4->DR This UART4 RX example could be modified to do TX. [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/UART%20with%20DMA%20mode&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=5544]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FUART%20with%20DMA%20mode&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=5544We’re moving the ST Community to a new platform to give you a better and more reliable community experience.