STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Start Problem on STM32F205

Posted on August 30, 2014 at 00:53I am attempting to communicate via I2C to another ST device (LPS331AP) and read its sensor values. However, I am not able to initiate the I2C session properly. On the wire, I can see that the start signal is actuall...

0690X000006058BQAQ.png
nate1 by Associate II
  • 4496 Views
  • 8 replies
  • 0 kudos

STM32F100R PB5 not enabling internal pull-up?

Posted on September 02, 2014 at 16:54Hello All,I've been bringing up some new hardware around an STM32F100RBT6 processor, and was planning on using PB5 as an input with an internal pull-up enabled. For some reason, none of my boards will enable the ...

Csma ca PLC EVALKITST7580

Posted on September 02, 2014 at 18:01Hello,Currently we are working on a custom board based on the power line modem demonstration kit (EVALKITST7580).I have question specifically regarding the firmware that we have received from ST of this evaluatio...

gnu by Associate II
  • 1067 Views
  • 1 replies
  • 0 kudos

VCP Problems with HAL Libraries and the STM32F4 Discovery

Posted on September 02, 2014 at 15:22Hi everybody,I have a problem with the VCP. I want to make a UART Connection between the STM-Board (STM32F4 Discovery) and my PC with the MicroUSB. Has anybody a working code for me. I know, I could use a UART In...

mathias by Associate II
  • 1213 Views
  • 1 replies
  • 0 kudos

Nucleo-F103RB and L3G4200D.

Posted on August 29, 2014 at 12:21 Hello I have a Nucleo-F103RB board and a EVK of L3G4200D. I am try connect this via I2C I have this code for config I2C void Inicializacion_uC(void) { RCC_Configuration_IO(); Inicial...

lemac by Associate III
  • 2318 Views
  • 6 replies
  • 0 kudos

Is STM32Cube speed optimized?

Posted on August 30, 2014 at 06:30I saw the code of stm32cube, It seems the code is not speed optimized,because nowadays micros have large amount of flash memory,the code size optimization is not important but speed optimization is very important, b...

Do I need a DMB instruction before starting DMA?

Posted on September 02, 2014 at 12:56I've been looking through the ARM documentation and am confused by when I need a DMB instruction. The CMSIS libraries for DMA(strm, enable) don't seem to include a DMB instruction, however the documentation indic...

Implement a usart1 receive interrupt without pressing a key

Posted on September 01, 2014 at 09:28Hello Forum,I have implemented a menu system on my app using the consoleMain Menu Select A ....1   (e.g. prints Debug1) Main Menu Select B.....2 2      Sub Menu B Select A ......1      Sub Menu B Select B.......2...

dvcosta43 by Associate II
  • 1619 Views
  • 3 replies
  • 0 kudos