Skip to main content
francescatodiego
Associate III
November 18, 2013
Question

SMTM32F4 ETH driver

  • November 18, 2013
  • 3 replies
  • 795 views
Posted on November 18, 2013 at 18:22

I am a beginner with STM32F4 and I am study the ETH driver procedure but I don't understand some instructions

For example:

  /* Clear MBC bits in the selected MAC address  high register */

  (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr)) &=(~(uint32_t)ETH_MACA1HR_MBC);

 

  /* Wait until the write operation will be taken into account :

   at least four TX_CLK/RX_CLK clock cycles */

  tmpreg = (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr));

  _eth_delay_(ETH_REG_WRITE_DELAY);

  (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr)) = tmpreg;

I don't understand the read and write same register after delay 

Thanks in advance for help

#stm32f4-eth
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
November 18, 2013
Posted on November 18, 2013 at 18:37

You'd need to find someone with a gate-level understanding of the design to talk to you, but the comments seem to suggest that there are consideration which fall under a different, slower, timing domain than the APB/AHB you are using to access the registers. ie pulling the bits off the wire, and checking the MAC address

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
eugene1
Visitor II
February 4, 2014
Posted on February 04, 2014 at 23:46

It's a silicone bug workaround. See latest errata sheet ''2.7.5 Successive write operations to the same register might not be fully taken into account''.

francescatodiego
Associate III
February 5, 2014
Posted on February 05, 2014 at 15:39

Thanks, thanks a lot trushkin now is clear