STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The I2C doesn't work! (STM32f030 and STM32f103)

Posted on September 02, 2014 at 18:54Hi ST partisans! (Wink) I have written two program for my two MCU. STM32F103RET6 and STM32f030. in the circuit, the STM32F030 should send ''Rohalamin'' string over I2C (as Master) . on the other hand, the STM32F1...

stm32f030: PF0/PF1 as GPIO

Posted on September 06, 2014 at 08:50 Dear forum members, I hope you can help solving a mystery. I stumbled upon these cute stm32f030f4 µCs and built minimalistic boards with it. No external oscillator used, thus pins PF0 and PF1 should b...

0690X00000602xiQAA.jpg
de_koepi by Associate II
  • 2226 Views
  • 1 replies
  • 0 kudos

STM32F4 SPI & Busy state

Posted on September 06, 2014 at 04:45Hello, I'm trying to handle the Chip Select pin via software, but I can't figure out how to determine when the SPI peripheral has finished the current transfer. By the looks of it, the SPI_SR_BSY flag, becomes 0 ...

shopping by Associate II
  • 750 Views
  • 0 replies
  • 0 kudos

STM32F411 VREF+ and VDDA Pinout Question

Posted on September 06, 2014 at 02:07Hello all,I am trying to confirm the pinout for Vref+ and VDDA on the STM32F411 products. The datasheet states if Vref+ is not available it is internally tied to VDDA. Only the UFBGA100L and LQFP100 packages expo...

STM32F0 spi clock problem

Posted on September 04, 2014 at 12:29 Hi! I'm trying to communicate with Atmel AT45DB081D dataflash over SPI. For testing I've send command to read Manufacturer and Device ID (0x9F on MOSI). After I've sent data, SPI clock stops to pulse...

zlajoan by Associate II
  • 2042 Views
  • 6 replies
  • 0 kudos

SOLVED!!! One Pulse on TIM15 on STM32F072/STM32072B-EVAL

Posted on September 03, 2014 at 23:55 Hi, I'm trying to modify the standard One Pulse example to use TIM15 to generate a delay, programmable width pulse, triggered by an external input. For the external input, I am using TIM3 routed to th...

rgrimes by Associate II
  • 2751 Views
  • 6 replies
  • 0 kudos

STM32F030 RTC wakeup from STOP mode

Posted on September 04, 2014 at 23:04I'm writing an app, that most of its time will spend in STOP or STANDBY mode (battery powered microsystem). I'd like the internal RTC to wakeup my STM32 every 5 minutes, enter the ISR, do its tasks in ISR (ADC me...

slatybor by Associate II
  • 1732 Views
  • 2 replies
  • 0 kudos

Two different DMA-Channels with same target?

Posted on September 03, 2014 at 07:15Hello, i was thinking about, if it would be possible to write to one peripherie register (for example the CCR1 of a Timer) with two different DMA-Channels. For sure not at the same time, but at different points ...

simple time scheduling-systick-stm32f407

Posted on September 04, 2014 at 11:34hi every body.i have a 6 or 7 sensors which all of them are connected my stm32f407 through ADC,Usart and i2c(kind of sensor fusion)i want to show the data of these sensors in pc through usart.i did this , but i j...

STM32L Max Voltage to FT pin while unpowered

Posted on August 01, 2014 at 02:45Can someone confirm if applying ~5.0V to a 5V tolerant pin on an STM32L151 while unpowered (VDD=0.0V) will damage it?The latest datasheets specify the Absolute Maximum Ratings are VDD+4.0V for FT pins, but bench tes...