STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f030 low-power

Posted on June 12, 2014 at 08:33Hi Did anybody try low-power modes on STM32f030 MCU? Specifically Stop mode. I can't get current under 200 uA. Did anybody succeed and get under this? If yes, please share how? I have disabled almost all of controller...

dejan2 by Associate
  • 2403 Views
  • 6 replies
  • 0 kudos

STM32f302RCT6 Y revision package marking problem

Posted on September 04, 2014 at 14:44Dear Forumers! I've just started to solder in the pcb components into my pcb. I have a MCU as in the title mentioned, and I've faced a problem about the chip placement. In the official drawing the package only co...

Using TIM1 as a PWM input

Posted on September 04, 2014 at 18:13 I am trying to set up TIM1 on my STM32F407 to act as a PWM input but I'm not having any luck. I have successfully used TIM2 with an identical circuit but when I modify the code to run on TIM1 I never get the...

keith by Associate
  • 1407 Views
  • 1 replies
  • 0 kudos

STM32F401 64pin pin1 marking / orientation

Posted on May 20, 2014 at 11:52I just want to place a STM32F401 64pin LQFP chip on my PCB, but to my surprise this chip has 2 pin 1 marking dots, on two diagonal corners. If I position the chip such, that I can read the text ''ARM STM32F401...'', th...

flyer31 by Senior
  • 9035 Views
  • 9 replies
  • 1 kudos

STM32F429 minimal schematic

Posted on August 08, 2014 at 17:21Hello! I'd like to design minimal schematic for STM32F429. I'd like to have all pins connected to goldpins. I want to program through ST-LINK and SWD. Please check my schematic. It's in the attachment. Thanks! #s...

erazmus by Associate
  • 3200 Views
  • 6 replies
  • 0 kudos

DISCOVERY BOARD SPI NO NSS

Posted on September 01, 2014 at 06:25Hello, I have a Discovery board and am using the SPI master DMA example and SPI4. I set NSS as SPI_NSS_HARD_OUTPUT. What I get is CLK, and MOSI come out perfectly, but NSS is pinned low. I put a pullup on it, and...

david2399 by Associate II
  • 2378 Views
  • 4 replies
  • 0 kudos

Run the STM32 System bootloader from application?

Posted on September 03, 2014 at 17:26I've been trying to run the system bootloader from my application on an STM32F205.  I think that should b feasible, but at present the system firmware behaves badly.  Probably I'm doing something wrong, but I can...

STM32F4 PSRAM configuration

Posted on September 03, 2014 at 10:26Hello, At the moment I am designing a PCB with the STM32F4 and PSRAM. Are the FSMC_NEx signals the bank switch signals? Can I use all the FSMC_NEx signals for the PSRAM or are certain banks only for a certain me...

0690X00000602xTQAQ.jpg
ad23 by Associate
  • 1463 Views
  • 1 replies
  • 0 kudos

STM32F103VC with MMCCard

Posted on September 01, 2014 at 17:11Hi,I want to use 512 Mb MMC card with STM32F103VC.Hardware is ok . Do you have any ideas on this issue? any driver for STM.How can I read and write file in MMC card ? Regards,

nafb by Associate II
  • 2103 Views
  • 5 replies
  • 0 kudos