cancel
Showing results for 
Search instead for 
Did you mean: 

Clock for AD7705BRZ from Microcontroller (STM32F100C4)

sovpeople
Associate
Posted on February 07, 2014 at 11:14

Hello!

I have some difficulties with my circuit developing. I don't have any crystall resonantor on my PCB but AD7705 need to be clocked externally. I've decided to use clock output from microcontroller (STM32F100). But I don't shure. Can you look at my scheme?

Thanks

#ad7705 #stm32f100
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on February 07, 2014 at 17:15

Just connect MCLKIN with the clock you're outputting via PA8

Do NOT connect MCLKOUT, and don't connected that back into the OSC IN/OUT of the STM32, it's pointless.

Connect the RESET for the AD7705BRZ to a GPIO pin on the STM32 you can control it, as PA8 isn't going to be generating a clock when you would normally start the system.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..