User Activity

Posted on July 22, 2015 at 15:35How to change mail id for this forum
Posted on July 20, 2015 at 07:39In stm32f030 Usart not working if I change starting address from 0x08000000 to 0x08003000. I mean the Usart Interrupt is not happening. The Usart is in Half duplex mode. If I used starting address as 0x08000000 Usart ...
Posted on March 16, 2015 at 12:02Hi Can anybody say me how to configure for USARt half duplex in stm32l15cb  . I have configured as I configured for stm32f030(working USART half duplex) but it did not work what are the changes between stm32f030 and ...
Posted on March 13, 2015 at 14:50Hi I have attached a piece of code in which DMA is configures as circular buffer. I have configured a total buffer complete interrupt. when I get into the interrupt I want to change the BUFF_SIZE In data shet it is ...
Posted on February 07, 2015 at 14:01I have a piece of code of usart half duplex which was working fine with stm32f030 mounted on the pcb (designed as required for my project) for some time . I am giving external 5 volt supply as I am driving motor t...
Kudos from