cancel
Showing results for 
Search instead for 
Did you mean: 

Discovery board programming problem

anand
Associate
Posted on February 06, 2014 at 11:54

I am using IAR with STM32-Value line discovery board. I am trying to program the kit but not getting programmed giving error like below,

 Fatal error: ST-Link DLL not found   Session aborted! 

 

Can any one guide me to rectify the problem.  I think there is some  in built ST-LINK

setting

 problem.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 06, 2014 at 13:30

The VL-Discovery uses an older version of the ST-LINK, Keil refers to this currently as ''ST-LINK (Deprecated)'', no idea what IAR does, but if there are two options, pick the older V1 version.

Failing that go download the appropriate drivers, and install them. Windows v8 will have it's own issues.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Senior
Posted on March 12, 2014 at 11:50

Please ensure that you have correctly installed ST-Link.

When using IAR toolchain for the first time , ST-Link Driver is required and shoud be installed. IAR setup doesn't install it automatically.

You can find it in this path ''C:\Program Files\IAR Systems\Embedded Workbench xxxx\arm\drivers\ST-Link''.