STM32F0XX analog watchdog config
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-03-11 8:50 AM
Posted on March 11, 2014 at 16:50
Hello everybody,
I'am trying to use analog watchdog on STM32F051K4 and I face some problems. I want to measure a pulse on PA0 (ADC_IN0) of 100us wide with an 1V amplitude above 0.5V offset. There is no example on this function for the F0. I tried to adapt F1 example without success yet.Here is the relevant code://threshold values for watchdog#define ADC_THR_H 0x708 //1V#define ADC_THR_L 0x5DC //0.88V /* GPIOB GPIO A Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOA, ENABLE); /* ADC1 Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);/*configure PA0 for ADC input*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);/*Enable interrupt on ADC Analog watchdog*/ NVIC_InitStructure.NVIC_IRQChannel = ADC1_COMP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); ADC_ClearITPendingBit(ADC1,ADC_IT_AWD); ADC_ITConfig(ADC1, ADC_IT_AWD, ENABLE);* Initialize ADC defaults */ /* ADC1 Configuration *******************************************************/ /* ADCs DeInit */ ADC_DeInit(ADC1); /* Configure the ADC1 with analog watchdog*/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_AnalogWatchdog_Channel_0; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; //ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward; //ADC_ChannelConfig(ADC1,ADC_Channel_0,ADC_SampleTime_1_5Cycles); ADC_Init(ADC1, &ADC_InitStructure); //Configure analog watchdog ADC_AnalogWatchdogSingleChannelConfig(ADC1, ADC_Channel_0); ADC_AnalogWatchdogThresholdsConfig(ADC1,ADC_THR_H,ADC_THR_L); ADC_AnalogWatchdogCmd(ADC1,ENABLE); ADC_AnalogWatchdogSingleChannelCmd(ADC1,ENABLE); ADC_StartOfConversion(ADC1); ADC_Cmd(ADC1,ENABLE);/*and my interrupt routine:*/void ADC1_COMP_IRQHandler(void){ if (ADC_GetITStatus(ADC1, ADC_IT_AWD)) { ADC_ClearFlag(ADC1, ADC_FLAG_AWD); ADC_ClearITPendingBit(ADC1, ADC_IT_AWD); if(ADC_threshold==0) ADC_threshold=1;}}In my main program, I check ADC_threshold value to light a led and I reset it.If somebody could help me, thanks.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-03-11 8:57 AM
Posted on March 11, 2014 at 16:57
There is no example on this function for the F0.
STM32F0xx_StdPeriph_Lib_V1.0.0\Project\STM32F0xx_StdPeriph_Examples\COMP\COMP_AnalogWatchdog\main.c STM32F0xx_StdPeriph_Lib_V1.0.0\Project\STM32F0xx_StdPeriph_Examples\ADC\ADC1_AnalogWatchdog\main.c
Tips, Buy me a coffee, or three.. PayPal Venmo
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
‎2014-03-11 9:07 AM
Posted on March 11, 2014 at 17:07
Sorry for this,
I looked in STM32F0-Discovery_FW_V1.0.0 only, I forgot STM32F0xx_StdPeriph_Lib_V1.3.1. and google didn't find anything about it.I check this, thanks