STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 F2/F4 USB Host issues

Posted on October 16, 2014 at 11:30 .ExternalClassE693089A00C04AC1B8142AED96FA644F p {margin-bottom:0.1in;line-height:120%;} Hi,I am writing a host stack and I have noticed various issues with the documentation and the hardware.Issue #1The pdf in...

miro_atc by Associate II
  • 947 Views
  • 1 replies
  • 0 kudos

Multiple interrupts

Posted on October 17, 2014 at 12:32Hello, would like to ask if say using interrupts to read from STM32 ADC and there is an external UART device that is read using uart interrupt also on STM32, would there be a case whereby the processing will be stu...

jephua by Associate II
  • 1192 Views
  • 2 replies
  • 0 kudos

STM32Cubemx+sd card with dma

Posted on October 16, 2014 at 12:24Hy all! I have a problem with CubeMX and sd card init with dma channels. I check that all of the sd card example project has 2 dma stream for sd card communication. So that I would like to set DMA2_Stream6 for Tx a...

totti001 by Associate II
  • 1624 Views
  • 3 replies
  • 0 kudos

Nucleo F103RB - Strange Flash Size

Posted on October 14, 2014 at 10:05Hi,i bought some Nucleo F103RB Boards and designed a circuit board for the Nucleo to drive my LEDs throught Bluetooth.The prototype with airwires worked perfectly, but know i tried it with my circuit and if i plug ...

sauer by Associate II
  • 3867 Views
  • 10 replies
  • 0 kudos

FATFS chan library wrong free space

Posted on October 16, 2014 at 18:46Good day everyone,I tried to use Chan's FatFS library for a while, it works fine,But I found some problems here.If I read free space in my MicroSD card, it reads it wrong.When I format it for a while it reads data ...

hitsumen by Associate II
  • 1877 Views
  • 1 replies
  • 0 kudos

stm32f4 dac software trigger

Posted on October 09, 2014 at 12:20  The original post was too long to process during our migration. Please click on the attachment to read the original post.

stzotter9 by Associate II
  • 7323 Views
  • 13 replies
  • 0 kudos

Issues with Getting started with the STM32L152D-EVAL

Posted on October 13, 2014 at 06:12Dear all, I started to work on a STM32L152D-EVAL board. While I started to play around, I tried the demonstration firmware from the following link: http://www.st.com/web/en/catalog/tools/PF257910 I am using the IA...

spveer by Associate II
  • 3779 Views
  • 14 replies
  • 0 kudos

Custom Bootloader HardFault

Posted on October 15, 2014 at 22:32Hi Folks,I wrote a custom bootloader at work and I'm getting a hard fault right at the instruction to jump to the Reset_Handler of the Application. This bootloader worked fine for 6 months but suddenly it started g...

ST-Link Utility slow to write EEPROM in newer versions

Posted on July 28, 2014 at 15:07Hello,We're currently using the ST-Link Utility CLI to program small production batches. We need to program some individual configuration bytes for each device, which we write to the EEPROM from a script using the ST-...

flash loader demostrator does not work with STM32F401CBU6

Posted on October 16, 2014 at 01:27I've a problem to connect Flash loader demonstrator to STM32F401CBU6. With any other device which I've used it's working without any problems. If I try to connect to STM32F401CBU6, I can connect, but at the stage o...

krestan by Associate II
  • 838 Views
  • 1 replies
  • 0 kudos