STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

flash loader demostrator does not work with STM32F401CBU6

Posted on October 16, 2014 at 01:27I've a problem to connect Flash loader demonstrator to STM32F401CBU6. With any other device which I've used it's working without any problems. If I try to connect to STM32F401CBU6, I can connect, but at the stage o...

krestan by Associate II
  • 834 Views
  • 1 replies
  • 0 kudos

Help to put together gcc-arm-none-eabi and STM32Cube

Posted on October 09, 2014 at 23:40Hello,I'm very new to STM32, I recently switched from Microchip platform and I'm working on a Mac (which seems to make everything harder).I followed this very nice tutorial http://www.davidrojas.co.uk/stm32f3discov...

STM32F101RD: Interrupt preemption not working

Posted on October 03, 2014 at 16:52System info: 8MHz external clock, 24MHz interrupt system clock.Interrupt preemption is not working for me no matter the combination of priorities and priority groupings. My goal is to have a high speed timer interr...

jansen by Associate II
  • 6032 Views
  • 18 replies
  • 0 kudos

I2C doesn't work!

Posted on October 15, 2014 at 11:38Please, help me into get out of this trouble!I' am working on discovery board STM32F429L-disco. In order to have an I2C available to drive an external device, I am using PC9 ad PA8 pins (I2C3), that are also used t...

giovanni2 by Associate II
  • 1645 Views
  • 2 replies
  • 0 kudos

STM32F3 ADC in differential mode

Posted on October 15, 2014 at 12:41The original post was too long to process during our migration. Please click on the attachment to read the original post.

nigel by Associate
  • 1929 Views
  • 3 replies
  • 0 kudos

Programming user option bytes

Posted on October 15, 2014 at 14:52 Hello, I would like to know if it is possible to change the value of the register FLASH_OPTCR by mapping a variable on it and to set the value in constant ? I think this is not possible because we need ...

fabien by Associate II
  • 2501 Views
  • 5 replies
  • 0 kudos

STM32F4 Discovery Vbat pin

Posted on October 15, 2014 at 14:48Hello.Where is a Vbat pin on a STM32F4 Discovery? How to connect external 3v3 battery on board? I use rtc.Best regards

Problems with USB CDC implementation on STM32F401CB

Posted on September 23, 2014 at 18:59Hello! I'm using the USB driver that is provided by STM32CubeMX 4.3.0. I want to use the CDC implemantation for virtual COM port communication between STM32F401CB and a PC. But I'm facing mainly two problems: 1.)...

tpoms9 by Associate II
  • 2014 Views
  • 3 replies
  • 0 kudos