STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TCS3200 color sensor with stm32f4

Posted on October 18, 2014 at 14:03Hi I'm trying to use TCS3200 color sensor interface with stm32f4I used input capture of timer 2, channel 3 and Interrupt to calculator pulse from OUT sensorOf course, i don't  know algorithm good. Because the senso...

41001051 by Associate II
  • 2457 Views
  • 1 replies
  • 0 kudos

STM32F429VG support 24-bit LCD TFT?

Posted on October 18, 2014 at 10:25Does STM32F429VG support 24-bit LCD TFT? It's 100 PIN LQFP and not has LCD_B1, LCD_R0, LCD_R1 pins definition in datasheet. So is it only support RGB565, and not support RGB888? Can you give me help?Thanks a lot.

ray by Associate II
  • 1435 Views
  • 3 replies
  • 0 kudos

FFT Programming(STM32f4xx)

Posted on October 18, 2014 at 08:04hi,Please someone post a sample example of fft program for stm32f4xx using cfft functions.  #learn-using-search-engines

STM32F4 what is the best I2C Comunication Method?

Posted on October 18, 2014 at 09:13Hello guys, a few months ago i started to work with discoveryF4 board and some sensors in i2c mode. But my inconvenient was that after several minutes or several hours the code just STONED... So in the last couple...

Bogdan by Senior
  • 798 Views
  • 1 replies
  • 0 kudos

ST-Link Connection error�

Posted on November 07, 2012 at 15:20I'm a student of University of Catania and I'm using IAR Embedded Workbench for ARM, v. 6.21, 32K Kickstart Edition on WIndows 7, for an university project to program a STM32F100XB board (using SWD Interface)It wo...

amedm by Associate II
  • 4011 Views
  • 10 replies
  • 0 kudos

externally triggered output compare

Posted on October 17, 2014 at 23:56I am using an STM32F4 discovery board.  I want to use an external trigger to generate an interrupt that will cause a pulse stream.  I have found examples using an external trigger for one pulse mode as well as outp...

garth by Associate
  • 802 Views
  • 1 replies
  • 0 kudos

MSC class USB device derived from STM32CUBEMX not enumerating

Posted on October 17, 2014 at 20:24I created a USB project using STM32CUBEMX ver 4.3 based on the Mass Storage Class for the STM32L0 Discovery Board. When I run the project that Cube creates out of the box on the Discovery board and connect it to my...

bnp979 by Associate III
  • 595 Views
  • 0 replies
  • 0 kudos

STM32L100C-DISCO USART Problems

Posted on October 02, 2014 at 06:04 Hi All, I'm new to embedded programming so I ordered one of these discovery boards to get my feet wet. I'm trying to get USART working so my first goal is to jump the TX and RX pins to see if I can send...

wprasek by Associate II
  • 4271 Views
  • 14 replies
  • 0 kudos

STM32F103 Usart 9-bit

Posted on October 17, 2014 at 01:02Hi guys, Sorry for my bad English. I would set up with 9-bit UART. So I want the UART interrupt only when I get a character with 9 bits. If I get the 8-bit character, I do not want to be interrupted. Is it possible...

rodrigo by Associate II
  • 4369 Views
  • 11 replies
  • 0 kudos

Stop mode: no entry

Posted on October 17, 2014 at 16:04 Hi at all, I'm working on an stm32401ccu, but I can't send it in stop mode; my code is quite simple, in fact I use the UART1 to send a command that realize the entry in stop mode, and a button linked to PB...

DUrbano by Associate III
  • 951 Views
  • 2 replies
  • 0 kudos