STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32429I-EVAL demonstration software

Posted on October 23, 2014 at 14:55hi all:    i have a STM32429I-EVAL but i can not find the  demonstration software in the ST web site, i can only donwload a cube software witch can not generate the demonstration software .why ST don't upload the  ...

LCD UC1608 SPI S8

Posted on November 02, 2012 at 13:17I have a problem with the initialization of the display AGG240128A05-FHW-R I do not know what could be wrong. Maybe someone has an idea? code:  &sharpinclude ''GLCD_240x128.h'' &sharpinclude ''STM32F10x.h''     ...

rudex by Associate
  • 1810 Views
  • 1 replies
  • 0 kudos

Unable to replicate hang when debugging with ST-LINK

Posted on October 26, 2014 at 04:44Our STM32F103 application hangs consistently within minutes under normal operation without the debugger, but when trying to debug running with ST-LINK SWD it doesn't hang (not using breakpoints).What is different w...

toddberk by Associate II
  • 951 Views
  • 1 replies
  • 0 kudos

STM32F407 Synchronised timers

Posted on October 24, 2014 at 15:56 I am trying to synchronise timer 3 and timer 4 to output a series of complimentary signals I have timer 3 outputting a square wave at 1MHz and I want timer 4 to output a square wave at 5kHz (factor of 1...

andrew23 by Associate II
  • 1214 Views
  • 1 replies
  • 0 kudos

Timer GPIO problem

Posted on October 25, 2014 at 15:36Hello everyone.I use STM32F4 Discovery. When I config timer (Time base) GPIO peripherals does not work. Timer is work, and GPIO is work (widthout timer configuration).Where is a problem?Best regards.

STM32F103 + SPI EEPROM without CS?

Posted on October 25, 2014 at 09:56Hello is possigle and problem free use serial SPI http://www.st.com/web/en/resource/technical/document/datasheet/CD00001441.pdfwith signal CS direcet on GND? Of course EEPROM is alone on this SPI bus.

victor23 by Associate
  • 873 Views
  • 1 replies
  • 0 kudos

ARM 32F4 Block Diagram

Posted on October 25, 2014 at 12:08 Dear all, The attached picture shows the ARM32F4 block diagram I mentioned three circles which i need more about them 1.CCM data RAM 64 KB 2.SRAM 112 KB 3.SRAM 16 KB What are the advantage to u...

0690X0000060MmnQAE.gif

STM32F407 ADC-DMA weird behaviour

Posted on October 24, 2014 at 21:58 I am using T2 to trigger ADC1,ADC2 and ADC3, all the ADCs are working in indepent mode. each ADC EOC will trigger a DMA2 in a dedicate channel. T2->ADC1->DMA2_Stream0.Channel_0 T2->ADC2->DMA2_Stream2.C...

gavinli by Associate II
  • 1108 Views
  • 1 replies
  • 0 kudos

STM32F4 running from sd card

Posted on October 24, 2014 at 20:07Hello, I wanted to know if it is possible to run a code on the stm32f4 board from an external flash like an sd card. Do I have to program a bootloader?Thanks