STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ulink2

Posted on November 08, 2014 at 21:27     IDE: Keil 4.74 (microvision)     Board: proprietary board with STM32F102C8     Program: only activates UART 1 to communicate with a terminal     1 - I can download the program to the board using the Flash Loa...

adaniel by Associate III
  • 2920 Views
  • 6 replies
  • 0 kudos

How to figure out my clock and pll clock ?

Posted on November 11, 2014 at 04:41 Hello All, and Clive, I've went back into the guts of my program after a long time being out of it, and I dont know how I can know the actual clock speed of my unit. I dont have a scope that does more tha...

Unexpected readings (2X or 0.5X) using ADC on STM32F0

Posted on November 10, 2014 at 20:07 I'm using the ADC on a STM32F072RBT6 to read a constant voltage that is derived from my supply voltage. Sometimes, I get a reading that is twice the expected value, and sometimes I get a reading that is half ...

Stm32f407 PPI communication with BLACK fin

Posted on November 10, 2014 at 13:16I want to write a code for PPI communication between stm32f407 and Blackfin .The code for blackfin I have got from open source...But I dont know how to write the same for stm32f407.Anybody have experience in doing...

sanjib by Associate III
  • 737 Views
  • 0 replies
  • 0 kudos

STORAGE_IsReady_HS() function contains garbage

Posted on September 23, 2014 at 01:55Hi AllCube 4.3.1/Keil/F4:When generating a cube project that includes a USB(HS) mass storage driver, if the file ''USBD_Storage_if.c'' already exists in your project AND has been modified within *USER CODE BEGIN*...

Using Internal Reference for ADC measurements

Posted on November 09, 2014 at 20:07Hi,I would like to use the internal reference (1,2 v) for ADC measurements on a STM32L151CC MCU ( 48 pin ). Is it possible? Thanks for your help.BR Per #internal-reference-adc

per23 by Associate
  • 865 Views
  • 1 replies
  • 0 kudos

GPIO_ToggleBits(GPIOD,GPIO_Pin_9);

Posted on November 09, 2014 at 12:46Dear All,I am using CMSIS '' STM32F0-Discovery_FW_V1.0.0 '' library files for STM32F0 MCU programming which does not support GPIO_ToggleBits(GPIOD,GPIO_Pin_9); instructionI already checked the ''gpio'' file which ...

pic_micro by Associate II
  • 1537 Views
  • 2 replies
  • 0 kudos